Common NVM driver Unit Test.
Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.
#include <stdint.h>
#include <stdbool.h>
#include <asf.h>
#include <string.h>
#include "common_nvm.h"
#include "conf_test.h"
Macros | |
#define | BYTE_PATTERN1(x) ((uint8_t)(((x) * 5 + 1) & 0xff)) |
Generates byte pattern 1 for a given address. More... | |
#define | BYTE_PATTERN2(x) ((uint8_t)(((x) * 3) & 0xff)) |
Generates byte pattern 2 for a given address. More... | |
Functions | |
int | main (void) |
Run common NVM driver unit tests. More... | |
static void | run_buffer_access_test (const struct test_case *test) |
Test the read and write buffer operations on the NVM. More... | |
static void | run_byte_access_test (const struct test_case *test) |
Test the read and write byte operations on the NVM. More... | |
static void | run_memory_check_test (const struct test_case *test) |
Performs a memory check on the non volatile memory. More... | |
#define BYTE_PATTERN1 | ( | x | ) | ((uint8_t)(((x) * 5 + 1) & 0xff)) |
Generates byte pattern 1 for a given address.
Referenced by run_byte_access_test().
#define BYTE_PATTERN2 | ( | x | ) | ((uint8_t)(((x) * 3) & 0xff)) |
Generates byte pattern 2 for a given address.
Referenced by run_buffer_access_test().
int main | ( | void | ) |
Run common NVM driver unit tests.
Initializes the clock system, board, serial output and NVM, then sets up the NVM unit test suite and runs it.
References usart_rs232_options::baudrate, board_init(), CONF_TEST_BAUDRATE, CONF_TEST_CHARLENGTH, CONF_TEST_PARITY, CONF_TEST_STOPBITS, CONF_TEST_USART, DEFINE_TEST_ARRAY, DEFINE_TEST_CASE, DEFINE_TEST_SUITE, run_buffer_access_test(), run_byte_access_test(), run_memory_check_test(), stdio_serial_init(), sysclk_init(), and test_suite_run().
|
static |
Test the read and write buffer operations on the NVM.
This function will test the read and write functionalities of the NVM using buffer access. It will first fill a buffer with a known pattern and read it back by testing each value read.
test | Current test case. |
References BYTE_PATTERN2, INT_FLASH, nvm_page_erase(), nvm_read(), nvm_write(), STATUS_OK, and test_assert_true.
Referenced by main().
|
static |
Test the read and write byte operations on the NVM.
This function will test the read and write functionalities of the NVM using byte access. It will first write a known pattern on the 2 consecutive addresses and read it back by testing each value read.
test | Current test case. |
References BYTE_PATTERN1, INT_FLASH, nvm_page_erase(), nvm_read_char(), nvm_write_char(), STATUS_OK, and test_assert_true.
Referenced by main().
|
static |
Performs a memory check on the non volatile memory.
This function will simply test the output of the function nvm_init and returns an error in case of failure.
test | Current test case. |
References INT_FLASH, nvm_init(), STATUS_OK, and test_assert_true.
Referenced by main().