Autonomous QTouch status type.
#include <touch_api_at32uc3l.h>
Data Fields | |
uint16_t | base_count |
uint16_t | current_count |
at_status_change_t | status_change |
uint16_t tag_touch_at_status_t::base_count |
The base count currently stored by the autonomous touch sensor.
This is useful for autonomous touch debugging purposes.
uint16_t tag_touch_at_status_t::current_count |
The current count acquired by the autonomous touch sensor.
This is useful for autonomous touch debugging purposes.
at_status_change_t tag_touch_at_status_t::status_change |
Autonomous QTouch Status change.
Referenced by touch_at_status_change_callback(), and touch_at_status_change_interrupt_callback().