Macros | |
#define | SET_PIN(x) (1u << (x)) |
Helper macro to include a selected pin. More... | |
Acquisition method manifest constants. | |
The following constants can be used to select the desired Touch acquisition methods to be used with the UC3L QTouch Library. Choose QMatrix, Autonomous QTouch, QTouch Group A and QTouch Group B methods by setting the corresponding macro to 1. It is possible for the QTouch Library to support one or more acquisition methods at the same time. For example, in order to use QMatrix and Autonomous QTouch acquisition methods at the same time, both DEF_TOUCH_QMATRIX and DEF_TOUCH_AUTONOMOUS_QTOUCH macros must be set to 1. | |
#define | DEF_TOUCH_QMATRIX (1) |
When 1, QMatrix method acquisition is used. More... | |
#define | DEF_TOUCH_AUTONOMOUS_QTOUCH (0) |
When 1, Autonomous QTouch method acquisition is used. More... | |
#define | DEF_TOUCH_QTOUCH_GRP_A (0) |
When 1, QTouch Group A method acquisition is used. More... | |
#define | DEF_TOUCH_QTOUCH_GRP_B (0) |
When 1, QTouch Group B method acquisition is used. More... | |
#define | DEF_TOUCH_QDEBUG_ENABLE_QM (1) |
Enable/Disable QDebug for touch debug information communication with QTouch Studio PC Software. More... | |
#define | DEF_TOUCH_QDEBUG_ENABLE_AT (0) |
#define | DEF_TOUCH_QDEBUG_ENABLE_QTA (0) |
#define | DEF_TOUCH_QDEBUG_ENABLE_QTB (0) |
#define | DEF_TOUCH_QDEBUG_ENABLE |
QMatrix Sensor Configuration options. | |
QMatrix Clock dependency note. The Example application uses a PBA clock of 48MHz. When the UC3L PBA Clock is changed to a different frequency, the following parameters must be changed accordingly to ensure proper QMatrix operation.
QMatrix resource requirement note. Caution:
| |
#define | QM_NUM_X_LINES (8u) |
QMatrix number of X Lines. More... | |
#define | QM_NUM_Y_LINES (8u) |
QMatrix number of Y Lines. More... | |
#define | QM_NUM_SENSORS (40u) |
QMatrix number of Sensors. More... | |
#define | QM_NUM_ROTORS_SLIDERS (8u) |
QMatrix number of Rotors and Sliders. More... | |
QMatrix Pin Configuration Options. | |
#define | QM_X_PINS_SELECTED |
QMatrix X Pins selected. More... | |
#define | QM_Y_PAIRS_SELECTED |
QMatrix Y-Yk Sense pairs selected. More... | |
#define | QM_SMP_DIS_PIN_OPTION (USE_NO_PIN) |
QMatrix SMP or DIS pin option. More... | |
#define | QM_VDIV_PIN_OPTION (USE_NO_PIN) |
QMatrix VDIV Pin option. More... | |
QMatrix Clock and Register Configuration Options. | |
#define | QM_GCLK_CAT_DIV (8u) |
QMatrix Generic clock (GCLK_CAT) divider for CAT. More... | |
#define | QM_CAT_CLK_DIV (5u) |
QMatrix CAT burst timing clock. More... | |
#define | QM_CHLEN (3u) |
QMatrix Charge Length. More... | |
#define | QM_SELEN (3u) |
QMatrix Settle Length. More... | |
#define | QM_CXDILEN (3u) |
QMatrix Cx Capacitor Discharge Length. More... | |
#define | QM_DILEN (255u) |
QMatrix Discharge Length. More... | |
#define | QM_DISHIFT (0u) |
QMatrix Discharge Shift. More... | |
#define | QM_MAX_ACQ_COUNT (3000u) |
QMatrix Maximum Count. More... | |
#define | QM_CONSEN (5u) |
QMatrix Consensus Filter Length. More... | |
#define | QM_INTREFSEL (1u) |
QMatrix Internal Reference Select. More... | |
#define | QM_INTVREFSEL (1u) |
QMatrix Internal Voltage Reference select. More... | |
#define | QM_ENABLE_SPREAD_SPECTRUM (1u) |
QMatrix Spread Spectrum Sensor Drive for QMatrix. More... | |
#define | QM_ENABLE_EXTERNAL_SYNC (0u) |
QMatrix External synchronization to reduce 50 or 60 Hz mains interference. More... | |
#define | QM_SYNC_TIM (0u) |
QMatrix Sync Time Interval. More... | |
QMatrix DMA Channel Options. | |
#define | QM_DMA_CHANNEL_0 (0u) |
QMatrix DMA Channel 0. More... | |
#define | QM_DMA_CHANNEL_1 (1u) |
QMatrix DMA Channel 1. More... | |
QMatrix Global acquisition parameters. | |
Refer the Touch Library User guide for more information on these parameters. | |
#define | QM_DI (4u) |
QMatrix Sensor detect integration (DI) limit. More... | |
#define | QM_NEG_DRIFT_RATE (20u) |
QMatrix Sensor negative drift rate. More... | |
#define | QM_POS_DRIFT_RATE (5u) |
QMatrix Sensor positive drift rate. More... | |
#define | QM_MAX_ON_DURATION (0u) |
QMatrix Sensor maximum on duration. More... | |
#define | QM_DRIFT_HOLD_TIME (20u) |
QMatrix Sensor drift hold time. More... | |
#define | QM_POS_RECAL_DELAY (10u) |
QMatrix Positive Recalibration delay. More... | |
#define | QM_RECAL_THRESHOLD (RECAL_50) |
QMatrix Sensor recalibration threshold. More... | |
QMatrix Callback functions. | |
#define | QM_FILTER_CALLBACK (qm_filter_callback) |
QMatrix Filter callback function. More... | |
Touch common configuration options. | |
#define | TOUCH_SYNC_PIN_OPTION (USE_NO_PIN) |
Touch Sync Pin option. More... | |
#define | TOUCH_SPREAD_SPECTRUM_MAX_DEV (4u) |
Touch Maximum Deviation. More... | |
#define | TOUCH_CSARES ((1u << 0u) | (1u << 2u) | (1u << 4u)) /* Enabling Resistive drive on X Lines. */ |
Touch Resistive Drive Enable for CSA lines. More... | |
#define | TOUCH_CSBRES ((1u << 0u) | (1u << 2u) | (1u << 4u) | (1u << 6u) | (1u << 8u)) /* Enabling Resistive drive on X Lines. */ |
Touch Resistive Drive Enable for CSB lines. More... | |
#define DEF_TOUCH_AUTONOMOUS_QTOUCH (0) |
When 1, Autonomous QTouch method acquisition is used.
When 0, Autonomous QTouch method acquisition is not used.
#define DEF_TOUCH_QDEBUG_ENABLE |
#define DEF_TOUCH_QDEBUG_ENABLE_AT (0) |
#define DEF_TOUCH_QDEBUG_ENABLE_QM (1) |
Enable/Disable QDebug for touch debug information communication with QTouch Studio PC Software.
The QTouch Library supports Autonomous QTouch, QMatrix, QTouch Group A/B modes at the sametime. However, when using QDebug, it is only possible to send the Touch debug information related to any one mode, at a given time. Only one among the DEF_TOUCH_QDEBUG_ENABLE_xx manifest constants below should be set to 1.
When 1, QDebug debug data communication to QTouch Studio is enabled. When 0, QDebug debug data communication to QTouch Studio is disabled.
#define DEF_TOUCH_QDEBUG_ENABLE_QTA (0) |
#define DEF_TOUCH_QDEBUG_ENABLE_QTB (0) |
#define DEF_TOUCH_QMATRIX (1) |
When 1, QMatrix method acquisition is used.
When 0, QMatrix method acquisition is not used.
#define DEF_TOUCH_QTOUCH_GRP_A (0) |
When 1, QTouch Group A method acquisition is used.
When 0, QTouch Group A method acquisition is not used.
#define DEF_TOUCH_QTOUCH_GRP_B (0) |
When 1, QTouch Group B method acquisition is used.
When 0, QTouch Group B method acquisition is not used.
#define QM_CAT_CLK_DIV (5u) |
QMatrix CAT burst timing clock.
The prescaler value is used to ensure that the CAT module clock (CLK_CAT) is divided to around 4 MHz to produce the burst timing clock. The prescaler uses the following formula to generate the burst timing clock: Burst timing clock = CLK_CAT / (2(DIV+1)) Range: 0u to 255u.
#define QM_CHLEN (3u) |
QMatrix Charge Length.
For QMatrix sensors, specifies how many burst prescaler clock cycles should be used for transferring charge to the sense capacitor. Units: Burst timing clock Range: 0u to 255u.
#define QM_CONSEN (5u) |
QMatrix Consensus Filter Length.
For QMatrix sensors, specifies that discharge will be terminated when CONSEN out of the most recent 5 comparator samples are positive. For example, a value of 3 in the CONSEN field will terminate discharge when 3 out of the most recent 5 comparator samples are positive. When CONSEN has the default value of 0, discharge will be terminated immediately when the comparator output goes positive. Range: 0u to 5u.
#define QM_CXDILEN (3u) |
QMatrix Cx Capacitor Discharge Length.
For QMatrix sensors, specifies how many burst prescaler clock cycles the CAT should use to discharge the Cx capacitor at the end of each burst cycle. Units: Burst timing clock Range: 0u to 255u.
#define QM_DI (4u) |
QMatrix Sensor detect integration (DI) limit.
Range: 0u to 255u.
#define QM_DILEN (255u) |
QMatrix Discharge Length.
For QMatrix sensors, specifies how many burst prescaler clock cycles the CAT should use to discharge the capacitors at the beginning of a burst sequence. Units: Burst timing clock Range: 0u to 255u.
#define QM_DISHIFT (0u) |
QMatrix Discharge Shift.
For QMatrix sensors, specifies how many bits the DILEN field should be shifted before using it to determine the discharge time. Range: 0u to 3u.
#define QM_DMA_CHANNEL_0 (0u) |
QMatrix DMA Channel 0.
Specify the DMA Channel option 0 to be used by the CAT module for transfer of Acquisition count from CAT register to memory. A different combination of DMA Channel option 0 and DMA Channel option 1 can be provided for each touch_qm_sensors_start_acquisition API call. Range: 0u to 11u. Note: DMA Channel option 0 and DMA Channel option 1 cannot be the same.
Referenced by main().
#define QM_DMA_CHANNEL_1 (1u) |
QMatrix DMA Channel 1.
Specify the DMA Channel option 1 to be used by the CAT module for transfer of burst length values from memory to CAT register. A different combination of DMA Channel option 0 and DMA Channel option 1 can be provided for each touch_qm_sensors_start_acquisition API call. Range: 0u to 11u. Note: DMA Channel option 0 and DMA Channel option 1 cannot be the same.
Referenced by main().
#define QM_DRIFT_HOLD_TIME (20u) |
QMatrix Sensor drift hold time.
Units: 200ms Default value: 20 (hold off drifting for 4 seconds after leaving detect). Range: 1u to 255u.
#define QM_ENABLE_EXTERNAL_SYNC (0u) |
QMatrix External synchronization to reduce 50 or 60 Hz mains interference.
0u: For QMatrix sensors, specifies that external synchronization is disabled. 1u: For QMatrix sensors, specifies that external synchronization mode is enabled using the TOUCH_SYNC_PIN_OPTION pin option provided. Refer TOUCH_SYNC_PIN_OPTION option.
#define QM_ENABLE_SPREAD_SPECTRUM (1u) |
QMatrix Spread Spectrum Sensor Drive for QMatrix.
0u: For QMatrix sensors, specifies that spread spectrum sensor drive shall not be used. 1u: For QMatrix sensors, specifies that spread spectrum sensor drive shall be used.
#define QM_FILTER_CALLBACK (qm_filter_callback) |
QMatrix Filter callback function.
A filter callback (when not NULL) is called by the Touch Library each time a new set of Signal values are available. An Example filter callback function prototype. void qm_filter_callback( touch_filter_data_t *p_filter_data );
#define QM_GCLK_CAT_DIV (8u) |
QMatrix Generic clock (GCLK_CAT) divider for CAT.
For proper QMatrix operation, the frequency of GCLK_CAT <= (PBA Clock/4). Range: 0u to 65535u. Note: The range specified is valid when this macro is used in conjunction with scif_gc_setup() API. Refer clock.c file. Note: This option is common for QMatrix, QTouch and Autonomous Touch methods of acquisition.
Referenced by init_clock(), and init_touch().
#define QM_INTREFSEL (1u) |
QMatrix Internal Reference Select.
This option is valid only when using the internal current sources mode of discharging the capacitors. 0u: The reference current flows through an external resistor on the DIS pin. 1u: The reference current flows through the internal reference resistor.
#define QM_INTVREFSEL (1u) |
QMatrix Internal Voltage Reference select.
This option is valid only when using the internal current sources mode of discharging the capacitors. 0u: The voltage for the reference resistor is generated from the internal band gap circuit. 1u: The voltage for the reference resistor is VDDIO/2.
#define QM_MAX_ACQ_COUNT (3000u) |
QMatrix Maximum Count.
For QMatrix sensors, specifies how many counts (signal value) the maximum acquisition should be. Range: 0u to 65535u.
#define QM_MAX_ON_DURATION (0u) |
QMatrix Sensor maximum on duration.
Units: 200ms (Example: a value 5u indicated Max ON duration of 1 second.) Default value: 0 (No maximum ON time limit). Range: 0u to 255u.
#define QM_NEG_DRIFT_RATE (20u) |
QMatrix Sensor negative drift rate.
Units: 200ms Default value: 20u = 4 seconds. Range: 1u to 127u.
#define QM_NUM_ROTORS_SLIDERS (8u) |
QMatrix number of Rotors and Sliders.
Specify the total number of QMatrix Rotors and Sliders to be used by the Touch Library. The number of Rotors and Sliders mentioned here is part of the Total number of sensors specified in the QM_NUM_SENSORS macro. Note: When no rotors or slider are required, specify a value of 0u.
#define QM_NUM_SENSORS (40u) |
QMatrix number of Sensors.
Specify the number of QMatrix touch sensors to be used by the Touch Library. A sensor can be a key, rotor or slider. Example configuration: If the configuration has 6 keys (a key is formed using one channel), one rotor (a QMatrix rotor is formed using 3 to 8 channels) and one slider (a QMatrix slider is formed using 3 to 8 channels), then the number of sensors is 6 key + 1 rotor + 1 slider = 8 sensors. Range: 1u to (number of X Lines * number of Y_Yk pairs).
#define QM_NUM_X_LINES (8u) |
QMatrix number of X Lines.
Specify the number of QMatrix X Lines to be used by the Touch Library. Refer CAT Matrix Connections Figure 28-2 in the datasheet. Range: 1u to 17u.
#define QM_NUM_Y_LINES (8u) |
QMatrix number of Y Lines.
Specify the number of QMatrix Y-Yk pair to be used by the Touch Library. Refer CAT Matrix Connections Figure 28-2 in the datasheet. Range: 1u to 8u.
#define QM_POS_DRIFT_RATE (5u) |
QMatrix Sensor positive drift rate.
Units: 200ms Default value: 5u = 1 second. Range: 1u to 127u.
#define QM_POS_RECAL_DELAY (10u) |
QMatrix Positive Recalibration delay.
Default value: 10. Range: 1u to 255u.
#define QM_RECAL_THRESHOLD (RECAL_50) |
QMatrix Sensor recalibration threshold.
Default: RECAL_50 (recalibration threshold = 50% of detection threshold). Range: refer recal_threshold_t enum in touch_api_at32uc3l.h.
#define QM_SELEN (3u) |
QMatrix Settle Length.
For QMatrix sensors, specifies how many burst prescaler clock cycles should be used for settling after charge transfer. Units: Burst timing clock Range: 0u to 255u.
#define QM_SMP_DIS_PIN_OPTION (USE_NO_PIN) |
QMatrix SMP or DIS pin option.
Specify the smp or dis pin option, if included in the hardware design. The QMatrix hardware can use a SMP pin for the discharge of the capacitors. In this arrangement, a logic-level (SMP) pin is connected to the capacitors through external high value resistors (typically between 100 kohm and 1 Megohm). When this arrangement is used, one of the SMP pin option must be chosen from the list available in the general_pin_options_t enum.
Alternatively, the UC3L CAT module provides an option of using the internal current sources for the discharge of capacitors. By choosing this hardware arrangement, the external resistors to be used with the SMP method can be avoided. The discharge of capacitors in this method can be done in two ways. If the INTREFSEL macro is set to 1, then a internal resistor shall be used to discharge the current. If the INTREFSEL macro is set to 0, then a external resistor shall be used to discharge the current. When the INTREFSEL=0 external discharge mode arrangement is used, one of the DIS pin option must be chosen from the list available in the general_pin_options_t enum. When the INTREFSEL=1 internal discharge mode arrangement is used, the USE_NO_PIN option must be specified for the QM_SMP_DIS_PIN_OPTION.
Refer general_pin_options_t enum in touch_api_at32uc3l.h file. Also, refer macros QM_INTREFSEL and QM_INTVREFSEL. Also, refer CAT Matrix Connections Figure 28-2 in the datasheet.
#define QM_SYNC_TIM (0u) |
QMatrix Sync Time Interval.
When non-zero, determines the number of prescaled clock cycles between the start of the acquisition on each X line for QMatrix acquisition. This option is valid only in the case when QM_ENABLE_EXTERNAL_SYNC is enabled. Units: Burst timing clock Range: 0u to 4095u.
#define QM_VDIV_PIN_OPTION (USE_NO_PIN) |
QMatrix VDIV Pin option.
Specify the vdiv pin option, if included in the hardware design. The VDIV pin provides an option to make ACREFN a small positive voltage in the case of any analog comparator offset issues. The VDIV pin is driven when the analog comparators are in use, and this signal can be used along with a voltage divider arrangement to create a small positive offset on the ACREFN pin.
Refer general_pin_options_t enum in touch_api_at32uc3l.h file. Also, refer CAT Matrix Connections Figure 28-2 in the datasheet.
#define QM_X_PINS_SELECTED |
QMatrix X Pins selected.
Specify the X lines to be used. Choose from X0 to X17. Setting Bit'n' indicates that a pin Xn is selected. Use the SET_PIN() macro to select the required X pin. Refer x_pin_options_t enum in touch_api_at32uc3l.h file.
#define QM_Y_PAIRS_SELECTED |
QMatrix Y-Yk Sense pairs selected.
Specify the Y pairs to be used. Choose from Y0_YK0 to Y7_YK7. Setting Bit'n' indicates that a pair Yn_YKn is selected. Use the SET_PIN() macro to select the required Yn_YKn pair. Refer y_pin_options_t enum in touch_api_at32uc3l.h file.
#define SET_PIN | ( | x | ) | (1u << (x)) |
Helper macro to include a selected pin.
#define TOUCH_CSARES ((1u << 0u) | (1u << 2u) | (1u << 4u)) /* Enabling Resistive drive on X Lines. */ |
Touch Resistive Drive Enable for CSA lines.
This option can be used to enable 1kOhm resistive drive capability, if available on a specific CSA pin. For the UC3L, the following CSA[n] pin have the resistive drive capability - CSARES: 0x0001AEEEu When bit n is 0, CSA[n] has the same drive properties as normal I/O pads. When bit n is 1, CSA[n] has a nominal output resistance of 1kOhm during the burst phase. Refer Table 28-2. Pin Selection Guide.
#define TOUCH_CSBRES ((1u << 0u) | (1u << 2u) | (1u << 4u) | (1u << 6u) | (1u << 8u)) /* Enabling Resistive drive on X Lines. */ |
Touch Resistive Drive Enable for CSB lines.
This option can be used to enable 1kOhm resistive drive capability, if available on a specific CSA pin. For the UC3L, the following CSB[n] pin have the resistive drive capability - CSBRES: 0x0000BEECu When bit n is 0, CSB[n] has the same drive properties as normal I/O pads. When bit n is 1, CSB[n] has a nominal output resistance of 1kOhm during the burst phase. Refer Table 28-2. Pin Selection Guide.
#define TOUCH_SPREAD_SPECTRUM_MAX_DEV (4u) |
Touch Maximum Deviation.
When spread spectrum burst is enabled using the QM_ENABLE_SPREAD_SPECTRUM option, MAX_DEV indicates the maximum number of prescaled clock cycles the burst pulse will be extended or shortened. Range: When only QMatrix is used, 0u to ((2u * QM_CAT_CLK_DIV) + 1u). Range: When only Autonomous QTouch is used, 0u to ((2u * AT_CAT_CLK_DIV) + 1u). Range: When only QTouch Group A is used, 0u to ((2u * QTA_CAT_CLK_DIV) + 1u). Range: When only QTouch Group B is used, 0u to ((2u * QTB_CAT_CLK_DIV) + 1u). Range: When a combination of QMatrix, Autonomous QTouch, QTouch Group A or QTouch Group B is used, 0u to ((2u * least of(QM_CAT_CLK_DIV, AT_CAT_CLK_DIV, QTA_CAT_CLK_DIV, QTB_CAT_CLK_DIV )) + 1u)
#define TOUCH_SYNC_PIN_OPTION (USE_NO_PIN) |
Touch Sync Pin option.
Specify the sync pin option, if included in the hardware design. To prevent interference from the 50 or 60 Hz mains line the CAT can trigger acquisition on the SYNC signal. The SYNC signal should be derived from the mains line. The acquisition will trigger on a falling edge of this signal. Refer general_pin_options_t enum in touch_api_at32uc3l.h file.