Macros | |
SD/MMC Status | |
Status List for the SD/MMC | |
#define | SD_MMC_REMOVED 0 |
#define | SD_MMC_INSERTED 1 |
#define | SD_MMC_REMOVING 2 |
Functions | |
Control Interface | |
Ctrl_status | sd_mmc_mci_test_unit_ready (uint8_t slot) |
Tests the memory state and initializes the memory if required. More... | |
Ctrl_status | sd_mmc_mci_test_unit_ready_0 (void) |
Instance Declaration for sd_mmc_mci_test_unit_ready Slot O. More... | |
Ctrl_status | sd_mmc_mci_test_unit_ready_1 (void) |
Instance Declaration for sd_mmc_mci_test_unit_ready Slot 1. More... | |
Ctrl_status | sd_mmc_mci_read_capacity (uint8_t slot, uint32_t *u32_nb_sector) |
Returns the address of the last valid sector in the memory. More... | |
Ctrl_status | sd_mmc_mci_read_capacity_0 (uint32_t *u32_nb_sector) |
Instance Declaration for sd_mmc_mci_read_capacity Slot O. More... | |
Ctrl_status | sd_mmc_mci_read_capacity_1 (uint32_t *u32_nb_sector) |
Instance Declaration for sd_mmc_mci_read_capacity Slot 1. More... | |
bool | sd_mmc_mci_wr_protect (uint8_t slot) |
Returns the write-protection state of the memory. More... | |
bool | sd_mmc_mci_wr_protect_0 (void) |
Instance Declaration for sd_mmc_mci_wr_protect Slot O. More... | |
bool | sd_mmc_mci_wr_protect_1 (void) |
Instance Declaration for sd_mmc_mci_wr_protect Slot 1. More... | |
bool | sd_mmc_mci_removal (uint8_t slot) |
Tells whether the memory is removable. More... | |
bool | sd_mmc_mci_removal_0 (void) |
Instance Declaration for sd_mmc_mci_removal Slot O. More... | |
bool | sd_mmc_mci_removal_1 (void) |
Instance Declaration for sd_mmc_mci_removal Slot 1. More... | |
MEM <-> RAM Interface | |
Ctrl_status | sd_mmc_mci_mem_2_ram (uint8_t slot, uint32_t addr, void *ram) |
Copies 1 data sector from the memory to RAM. More... | |
Ctrl_status | sd_mmc_mci_dma_mem_2_ram (uint8_t slot, uint32_t addr, void *ram) |
Ctrl_status | sd_mmc_mci_mem_2_ram_0 (uint32_t addr, void *ram) |
Instance Declaration for sd_mmc_mci_mem_2_ram Slot O. More... | |
Ctrl_status | sd_mmc_mci_mem_2_ram_1 (uint32_t addr, void *ram) |
Instance Declaration for sd_mmc_mci_mem_2_ram Slot 1. More... | |
Ctrl_status | sd_mmc_mci_ram_2_mem (uint8_t slot, uint32_t addr, const void *ram) |
Copies 1 data sector from RAM to the memory. More... | |
Ctrl_status | sd_mmc_mci_dma_ram_2_mem (uint8_t slot, uint32_t addr, const void *ram) |
Ctrl_status | sd_mmc_mci_ram_2_mem_0 (uint32_t addr, const void *ram) |
Instance Declaration for sd_mmc_mci_mem_2_ram Slot O. More... | |
Ctrl_status | sd_mmc_mci_ram_2_mem_1 (uint32_t addr, const void *ram) |
Instance Declaration for sd_mmc_mci_mem_2_ram Slot 1. More... | |
Ctrl_status | sd_mmc_mci_multiple_mem_2_ram (uint8_t slot, uint32_t addr, void *ram, uint32_t nb_sectors) |
Copies nb_sectors data sector from the memory to RAM. More... | |
Ctrl_status | sd_mmc_mci_dma_multiple_mem_2_ram (uint8_t slot, uint32_t addr, void *ram, uint32_t nb_sectors) |
Ctrl_status | sd_mmc_mci_multiple_mem_2_ram_0 (uint32_t addr, void *ram, uint32_t nb_sectors) |
Instance Declaration for sd_mmc_mci_mem_2_ram Slot O. More... | |
Ctrl_status | sd_mmc_mci_multiple_mem_2_ram_1 (uint32_t addr, void *ram, uint32_t nb_sectors) |
Instance Declaration for sd_mmc_mci_mem_2_ram Slot 1. More... | |
Ctrl_status | sd_mmc_mci_multiple_ram_2_mem (uint8_t slot, uint32_t addr, const void *ram, uint32_t nb_sectors) |
Copies nb_sectors data sector from RAM to the memory. More... | |
Ctrl_status | sd_mmc_mci_dma_multiple_ram_2_mem (uint8_t slot, uint32_t addr, const void *ram, uint32_t nb_sectors) |
Ctrl_status | sd_mmc_mci_multiple_ram_2_mem_0 (uint32_t addr, const void *ram, uint32_t nb_sectors) |
Instance Declaration for sd_mmc_mci_mem_2_ram Slot O. More... | |
Ctrl_status | sd_mmc_mci_multiple_ram_2_mem_1 (uint32_t addr, const void *ram, uint32_t nb_sectors) |
Instance Declaration for sd_mmc_mci_mem_2_ram Slot 1. More... | |