Loading [MathJax]/extensions/tex2jax.js

Microchip® Advanced Software Framework

usart.h File Reference
#include <avr32/io.h>
#include "compiler.h"

Data Structures

struct  usart_iso7816_options_t
 Input parameters when initializing ISO7816 mode. More...
 
struct  usart_options_t
 Input parameters when initializing RS232 and similar modes. More...
 

Macros

#define USART_DEFAULT_TIMEOUT   10000
 Default time-out value (number of attempts). More...
 
Return Values
#define USART_SUCCESS   0
 Successful completion. More...
 
#define USART_FAILURE   -1
 Failure because of some unspecified reason. More...
 
#define USART_INVALID_INPUT   1
 Input value out of range. More...
 
#define USART_INVALID_ARGUMENT   -1
 Argument value out of range. More...
 
#define USART_TX_BUSY   2
 Transmitter was busy. More...
 
#define USART_RX_EMPTY   3
 Nothing was received. More...
 
#define USART_RX_ERROR   4
 Transmission error occurred. More...
 
#define USART_MODE_FAULT   5
 USART not in the appropriate mode. More...
 
Parity Settings
#define USART_EVEN_PARITY   AVR32_USART_MR_PAR_EVEN
 Use even parity on character transmission. More...
 
#define USART_ODD_PARITY   AVR32_USART_MR_PAR_ODD
 Use odd parity on character transmission. More...
 
#define USART_SPACE_PARITY   AVR32_USART_MR_PAR_SPACE
 Use a space as parity bit. More...
 
#define USART_MARK_PARITY   AVR32_USART_MR_PAR_MARK
 Use a mark as parity bit. More...
 
#define USART_NO_PARITY   AVR32_USART_MR_PAR_NONE
 Don't use a parity bit. More...
 
#define USART_MULTIDROP_PARITY   AVR32_USART_MR_PAR_MULTI
 Parity bit is used to flag address characters. More...
 
Stop Bits Settings
#define USART_1_STOPBIT   AVR32_USART_MR_NBSTOP_1
 Use 1 stop bit. More...
 
#define USART_1_5_STOPBITS   AVR32_USART_MR_NBSTOP_1_5
 Use 1.5 stop bits. More...
 
#define USART_2_STOPBITS   AVR32_USART_MR_NBSTOP_2
 Use 2 stop bits (for more, just give the number of bits). More...
 
Channel Modes
#define USART_NORMAL_CHMODE   AVR32_USART_MR_CHMODE_NORMAL
 Normal communication. More...
 
#define USART_AUTO_ECHO   AVR32_USART_MR_CHMODE_ECHO
 Echo data. More...
 
#define USART_LOCAL_LOOPBACK   AVR32_USART_MR_CHMODE_LOCAL_LOOP
 Local loopback. More...
 
#define USART_REMOTE_LOOPBACK   AVR32_USART_MR_CHMODE_REMOTE_LOOP
 Remote loopback. More...
 

Functions

Initialization Functions
void usart_reset (volatile avr32_usart_t *usart)
 Resets the USART and disables TX and RX. More...
 
int usart_init_rs232 (volatile avr32_usart_t *usart, const usart_options_t *opt, long pba_hz)
 Sets up the USART to use the standard RS232 protocol. More...
 
int usart_init_rs232_tx_only (volatile avr32_usart_t *usart, const usart_options_t *opt, long pba_hz)
 Sets up the USART to use the standard RS232 protocol in TX-only mode. More...
 
int usart_init_hw_handshaking (volatile avr32_usart_t *usart, const usart_options_t *opt, long pba_hz)
 Sets up the USART to use hardware handshaking. More...
 
int usart_init_modem (volatile avr32_usart_t *usart, const usart_options_t *opt, long pba_hz)
 Sets up the USART to use the modem protocol, activating dedicated inputs/outputs. More...
 
int usart_init_sync_master (volatile avr32_usart_t *usart, const usart_options_t *opt, long pba_hz)
 Sets up the USART to use a synchronous RS232-like protocol in master mode. More...
 
int usart_init_sync_slave (volatile avr32_usart_t *usart, const usart_options_t *opt, long pba_hz)
 Sets up the USART to use a synchronous RS232-like protocol in slave mode. More...
 
int usart_init_rs485 (volatile avr32_usart_t *usart, const usart_options_t *opt, long pba_hz)
 Sets up the USART to use the RS485 protocol. More...
 
int usart_init_IrDA (volatile avr32_usart_t *usart, const usart_options_t *opt, long pba_hz, unsigned char irda_filter)
 Sets up the USART to use the IrDA protocol. More...
 
int usart_init_iso7816 (volatile avr32_usart_t *usart, const usart_iso7816_options_t *opt, int t, long pba_hz)
 Sets up the USART to use the ISO7816 T=0 or T=1 smartcard protocols. More...
 
Read and Reset Error Status Bits
static __always_inline void usart_reset_status (volatile avr32_usart_t *usart)
 Resets the error status. More...
 
static __always_inline int usart_parity_error (volatile avr32_usart_t *usart)
 Checks if a parity error has occurred since last status reset. More...
 
static __always_inline int usart_framing_error (volatile avr32_usart_t *usart)
 Checks if a framing error has occurred since last status reset. More...
 
static __always_inline int usart_overrun_error (volatile avr32_usart_t *usart)
 Checks if an overrun error has occurred since last status reset. More...
 
ISO7816 Control Functions
static __always_inline void usart_iso7816_enable_receiver (volatile avr32_usart_t *usart)
 Enables the ISO7816 receiver. More...
 
static __always_inline void usart_iso7816_enable_transmitter (volatile avr32_usart_t *usart)
 Enables the ISO7816 transmitter. More...
 
Transmit/Receive Functions
int usart_send_address (volatile avr32_usart_t *usart, int address)
 Addresses a receiver. More...
 
static __always_inline int usart_tx_ready (volatile avr32_usart_t *usart)
 Tests if the USART is ready to transmit a character. More...
 
int usart_write_char (volatile avr32_usart_t *usart, int c)
 Writes the given character to the TX buffer if the transmitter is ready. More...
 
static __always_inline void usart_bw_write_char (volatile avr32_usart_t *usart, int c)
 An active wait writing a character to the USART. More...
 
int usart_putchar (volatile avr32_usart_t *usart, int c)
 Sends a character with the USART. More...
 
static __always_inline int usart_tx_empty (volatile avr32_usart_t *usart)
 Tests if all requested USART transmissions are over. More...
 
static __always_inline int usart_test_hit (volatile avr32_usart_t *usart)
 Tests if the USART contains a received character. More...
 
int usart_read_char (volatile avr32_usart_t *usart, int *c)
 Checks the RX buffer for a received character, and stores it at the given memory location. More...
 
int usart_getchar (volatile avr32_usart_t *usart)
 Waits until a character is received, and returns it. More...
 
void usart_write_line (volatile avr32_usart_t *usart, const char *string)
 Writes one character string to the USART. More...
 
int usart_get_echo_line (volatile avr32_usart_t *usart)
 Gets and echoes characters until end of line (detected by a CR character). More...