#include "compiler.h"
Data Structures | |
struct | eic_options_t |
Configuration parameters of the EIC module. More... | |
Macros | |
External Interrupt lines | |
#define | EXT_INT0 AVR32_EIC_INT0 |
Line 0. More... | |
#define | EXT_INT1 AVR32_EIC_INT1 |
Line 1. More... | |
#define | EXT_INT2 AVR32_EIC_INT2 |
Line 2. More... | |
#define | EXT_INT3 AVR32_EIC_INT3 |
Line 3. More... | |
#define | EXT_INT4 AVR32_EIC_INT4 |
Line 4. More... | |
#define | EXT_INT5 AVR32_EIC_INT5 |
Line 5. More... | |
#define | EXT_INT6 AVR32_EIC_INT6 |
Line 6. More... | |
#define | EXT_INT7 AVR32_EIC_INT7 |
Line 7. More... | |
#define | EXT_NMI AVR32_EIC_NMI |
Line 8. More... | |
Mode Trigger Options | |
#define | EIC_MODE_EDGE_TRIGGERED AVR32_EIC_EDGE_IRQ |
#define | EIC_MODE_LEVEL_TRIGGERED AVR32_EIC_LEVEL_IRQ |
Edge level Options | |
#define | EIC_EDGE_FALLING_EDGE AVR32_EIC_FALLING_EDGE |
#define | EIC_EDGE_RISING_EDGE AVR32_EIC_RISING_EDGE |
Level Options | |
#define | EIC_LEVEL_LOW_LEVEL AVR32_EIC_LOW_LEVEL |
#define | EIC_LEVEL_HIGH_LEVEL AVR32_EIC_HIGH_LEVEL |
Filter Options | |
#define | EIC_FILTER_ENABLED AVR32_EIC_FILTER_ON |
#define | EIC_FILTER_DISABLED AVR32_EIC_FILTER_OFF |
Synch Mode Options | |
#define | EIC_SYNCH_MODE AVR32_EIC_SYNC |
#define | EIC_ASYNCH_MODE AVR32_EIC_USE_ASYNC |
Functions | |
void | eic_disable_line (volatile avr32_eic_t *eic, uint32_t line_number) |
Disable the EIC driver. More... | |
void | eic_disable_lines (volatile avr32_eic_t *eic, uint32_t mask_lines) |
Disable the EIC driver. More... | |
void | eic_enable_line (volatile avr32_eic_t *eic, uint32_t line_number) |
Enable the EIC driver. More... | |
void | eic_enable_lines (volatile avr32_eic_t *eic, uint32_t mask_lines) |
Enable the EIC driver. More... | |
void | eic_init (volatile avr32_eic_t *eic, const eic_options_t *opt, uint32_t nb_lines) |
Init the EIC driver. More... | |
bool | eic_is_line_enabled (volatile avr32_eic_t *eic, uint32_t line_number) |
Tells whether an EIC line is enabled. More... | |
Interrupt Control Functions | |
void | eic_enable_interrupt_lines (volatile avr32_eic_t *eic, uint32_t mask_lines) |
Enable the interrupt feature of the EIC. More... | |
void | eic_enable_interrupt_line (volatile avr32_eic_t *eic, uint32_t line_number) |
Enable the interrupt feature of the EIC. More... | |
void | eic_disable_interrupt_lines (volatile avr32_eic_t *eic, uint32_t mask_lines) |
Disable the interrupt feature of the EIC. More... | |
void | eic_disable_interrupt_line (volatile avr32_eic_t *eic, uint32_t line_number) |
Disable the interrupt feature of the EIC. More... | |
bool | eic_is_interrupt_line_enabled (volatile avr32_eic_t *eic, uint32_t line_number) |
Tells whether an EIC interrupt line is enabled. More... | |
void | eic_clear_interrupt_lines (volatile avr32_eic_t *eic, uint32_t mask_lines) |
Clear the interrupt flag. Call this function once you've handled the interrupt. More... | |
void | eic_clear_interrupt_line (volatile avr32_eic_t *eic, uint32_t line_number) |
Clear the interrupt flag. Call this function once you've handled the interrupt. More... | |
bool | eic_is_interrupt_line_pending (volatile avr32_eic_t *eic, uint32_t line_number) |
Tells whether an EIC interrupt line is pending. More... | |
void | eic_enable_interrupt_scan (volatile avr32_eic_t *eic, uint32_t presc) |
Enable the interrupt scan feature of the EIC. More... | |
void | eic_disable_interrupt_scan (volatile avr32_eic_t *eic) |
Disable the interrupt scan feature of the EIC. More... | |
uint32_t | eic_get_interrupt_pad_scan (volatile avr32_eic_t *eic) |
Return scan pad number that causes interrupt. More... | |