Macros | |
#define | PM_NOT_SUPPORTED (-10000) |
Define "not supported" for the power manager features. More... | |
#define | PM_POLL_TIMEOUT 100000 |
The timeguard used for polling (expressed in ticks). More... | |
#define | PM_UNLOCK(reg) (AVR32_PM.unlock = (unsigned long)(AVR32_PM_UNLOCK_KEY_VALUE << AVR32_PM_UNLOCK_KEY_OFFSET)|(reg)) |
Unlock PM register macro. More... | |
Enumerations | |
enum | pm_clk_domain_t { PM_CLK_DOMAIN_0 = AVR32_PM_CLK_GRP_CPU, PM_CLK_DOMAIN_1 = AVR32_PM_CLK_GRP_HSB, PM_CLK_DOMAIN_2 = AVR32_PM_CLK_GRP_PBA, PM_CLK_DOMAIN_3 = AVR32_PM_CLK_GRP_PBB, PM_CLK_DOMAIN_INVALID } |
The clock domains of the power manager. More... | |
enum | pm_clk_src_t { PM_CLK_SRC_SLOW = AVR32_PM_MCSEL_SLOW, PM_CLK_SRC_OSC0 = AVR32_PM_MCSEL_OSC0, PM_CLK_SRC_DFLL0 = AVR32_PM_MCSEL_DFLL0, PM_CLK_SRC_RC120M = AVR32_PM_MCSEL_RC120M, PM_CLK_SRC_INVALID } |
Device-specific data. More... | |
enum | pm_divratio_max_t { PM_CPUSEL_DIVRATIO_MAX = AVR32_PM_CPUSEL_CPUSEL_MASK >> AVR32_PM_CPUSEL_CPUSEL_OFFSET, PM_HSBSEL_DIVRATIO_MAX = AVR32_PM_HSBSEL_HSBSEL_MASK >> AVR32_PM_HSBSEL_HSBSEL_OFFSET, PM_PBASEL_DIVRATIO_MAX = AVR32_PM_PBASEL_PBSEL_MASK >> AVR32_PM_PBASEL_PBSEL_OFFSET, PM_PBBSEL_DIVRATIO_MAX = AVR32_PM_PBBSEL_PBSEL_MASK >> AVR32_PM_PBBSEL_PBSEL_OFFSET } |
The maximum synchronous clock division ratio for each clock domain. More... | |
enum | pm_divratio_t { PM_CKSEL_DIVRATIO_2 = 0, PM_CKSEL_DIVRATIO_4, PM_CKSEL_DIVRATIO_8, PM_CKSEL_DIVRATIO_16, PM_CKSEL_DIVRATIO_32, PM_CKSEL_DIVRATIO_64, PM_CKSEL_DIVRATIO_128, PM_CKSEL_DIVRATIO_256, PM_CKSEL_DIVRATIO_ERROR } |
The possible synchronous clock division ratio. More... | |
Functions | |
Clock Functions | |
long | pm_set_mclk_source (pm_clk_src_t src) |
Set the main clock. More... | |
long | pm_config_mainclk_safety (bool cfd, bool ocp, bool final) |
Configure the main clock safety mechanisms. More... | |
long | pm_set_clk_domain_div (pm_clk_domain_t clock_domain, pm_divratio_t divratio) |
Set the division ratio for a clock domain. More... | |
long | pm_disable_clk_domain_div (pm_clk_domain_t clock_domain) |
Disable the division ratio for a clock domain. More... | |
void | pm_set_all_cksel (unsigned long main_clock_f_hz, unsigned long cpu_f_hz, unsigned long pba_f_hz, unsigned long pbb_f_hz) |
Enable or Disable the division ratio for each clock domain depending on the main source clock frequency and each clock domain target frequency. More... | |
long | pm_wait_for_clk_ready (void) |
Wait actively for the clock settings to be effective. More... | |
Module Functions | |
long | pm_enable_module (unsigned long module) |
Enable the clock of a module. More... | |
long | pm_disable_module (unsigned long module) |
Disable the clock of a module. More... | |
Reset Functions | |
static __always_inline unsigned long | pm_get_reset_cause (void) |
Returns MCU last reset cause. More... | |
Interrupt Functions | |
static __always_inline void | pm_enable_interrupts (unsigned long mask) |
Enable power manager interrupts. More... | |
static __always_inline void | pm_disable_interrupts (unsigned long mask) |
Disable power manager interrupts. More... | |
static __always_inline unsigned long | pm_get_enabled_interrupts (void) |
Read the enabled power manager interrupts. More... | |
static __always_inline unsigned long | pm_get_interrupts_status (void) |
Read the interrupts status of the power manager. More... | |
static __always_inline void | pm_clear_interrupt_status (unsigned long mask) |
Clear raised interrupts from the power manager. More... | |
Misc Functions | |
static __always_inline unsigned long | pm_get_status (void) |
Get the PM status. More... | |
Sleep Functions | |
#define | SLEEP(sleep_mode) {__asm__ __volatile__ ("sleep "STRINGZ(sleep_mode));} |
Sets the MCU in the specified sleep mode. More... | |
static __always_inline unsigned long | pm_get_wake_cause (void) |
Returns MCU wake cause. More... | |
static __always_inline void | pm_asyn_wake_up_enable (unsigned long awen_mask) |
Enable one or several asynchronous wake-up source. More... | |
static __always_inline void | pm_asyn_wake_up_disable (unsigned long awen_mask) |
Disable one or several asynchronous wake-up sources. More... | |