Macros | |
#define | CLASS_SUBCLASS_PROTOCOL {VENDOR_CLASS, NO_SUBCLASS, NO_PROTOCOL} |
CLASS/SUBCLASS/PROTOCOL supported table list. More... | |
#define | DEVICE_ADDRESS 0x05 |
The address that will be assigned to the connected device. More... | |
#define | EP_TEMP_IN 1 |
#define | EP_TEMP_OUT 2 |
#define | HOST_AUTO_CFG_ENDPOINT ENABLE |
Try to configure the host pipe according to the device descriptors received. More... | |
#define | HOST_CONTINUOUS_SOF_INTERRUPT DISABLE |
Host Start-of-Frame interrupt always enabled. More... | |
#define | Host_device_class_not_supported_action() |
#define | Host_device_connection_action() |
#define | Host_device_disconnection_action() (tpl_new_device_connected = false) |
#define | Host_device_error_action() |
#define | Host_device_not_supported_action() |
#define | Host_device_supported_action() |
#define | HOST_ERROR_RESTART ENABLE |
When host error state detected, go to detached state. More... | |
#define | Host_hwup_action() |
#define | Host_new_device_connection_action() (tpl_new_device_connected = true) |
#define | Host_sof_action() host_sof_action() |
#define | HOST_STRICT_VID_PID_TABLE DISABLE |
The host controller will be limited to the strict VID/PID list. More... | |
#define | Host_suspend_action() |
#define | Host_user_check_class_action(x) |
During the verification of the device class by the host (after device enumeration), this call-back function allows to look more deeply into the configuration descriptor. More... | |
#define | ID_PIN_CHANGE_GENERATE_RESET ENABLE |
Force CPU reset upon ID pin change. More... | |
#define | LOG_STR(str) print_dbg(str) |
Debug trace macro. More... | |
#define | MAX_EP_PER_INTERFACE 3 |
The maximal number of endpoints per interface supported. More... | |
#define | MAX_INTERFACE_SUPPORTED 0x02 |
The maximal number of interfaces that can be supported (composite device) More... | |
#define | NAK_RECEIVE_TIMEOUT 0x0010 |
Number of NAK handshakes before time-out for receive functions (up to 0xFFFF) More... | |
#define | NAK_SEND_TIMEOUT 0x0010 |
Number of NAK handshakes before time-out for transmit functions (up to 0xFFFF) More... | |
#define | NAK_TIMEOUT_ENABLE ENABLE |
Enable cpt NAK time-out for host transfer. More... | |
#define | NB_ENDPOINTS 3 |
#define | SIZEOF_DATA_STAGE 250 |
The size of RAM buffer reserved for descriptor handling. More... | |
#define | TIMEOUT_DELAY 1 |
Delay 1/4 s (250 ms) before time-out value. More... | |
#define | TIMEOUT_DELAY_ENABLE ENABLE |
Enable time-out delay for host transfer. More... | |
#define | USB_DEVICE_FEATURE true |
ENABLE to activate the device software framework support. More... | |
#define | USB_HOST_FEATURE true |
ENABLE to activate the host software framework support. More... | |
#define | USB_HOST_PIPE_INTERRUPT_TRANSFER DISABLE |
USB host pipes transfers use USB communication interrupt (allows to use non-blocking functions) When set to ENABLE, take care of the NAK_RECEIVE_TIMEOUT value: NAK OUT will be counted faster and a timeout will occur if using FreeRTOS, since host and device tasks are sleeping several milliseconds. More... | |
#define | Usb_id_transition_action() |
#define | USB_INT_LEVEL AVR32_INTC_INT0 |
USB interrupt priority level. More... | |
#define | Usb_reset_action() |
#define | Usb_resume_action() |
#define | Usb_set_configuration_action() |
#define | Usb_sof_action() usb_sof_action() |
#define | Usb_suspend_action() |
#define | Usb_vbus_off_action() |
#define | Usb_vbus_on_action() |
#define | Usb_wake_up_action() |
#define | VID_PID_TABLE {ATMEL_VID, 1, ENUM_EXAMPLE_PID} |
VID/PID supported table list. More... | |
Functions | |
void | host_sof_action (void) |
host_sof_action More... | |
void | host_suspend_action (void) |
void | usb_sof_action (void) |
usb_sof_action More... | |
void | usb_suspend_action (void) |
Variables | |
volatile bool | tpl_new_device_connected |