Type by which tasks are referenced. For example, a call to xTaskCreate returns (via a pointer parameter) an xTaskHandle variable that can then be used as a parameter to vTaskDelete to delete the task.
Generated on Sat Mar 5 2022 00:30:57 for USBB device enumeration and host example with FreeRTOS for evk1104 (from ASF V1) by 1.8.5