Type by which tasks are referenced. For example, a call to xTaskCreate returns (via a pointer parameter) an xTaskHandle variable that can then be used as a parameter to vTaskDelete to delete the task.
Generated on Sat Mar 5 2022 01:15:02 for USBB Enumeration Example with FreeRTOS for evk1105 (from ASF V1) by 1.8.5