This script is used to visualize a data stream from the serial port formatted as follow:
This script is a combination of two main programs (Data Get and Data Print)
You can also directly modify two parameters in the script:
Once launched, the script will wait until a reset has been performed on the target (which means it will wait until the beginning of the transmission to be sure data are well synchronized).
All the files related to this module are located under /avr32/services/dsp/dsplib/utils/scripts/serial_scope