#include "fs_com.h"
Data Structures | |
struct | Fs_clusterlist_cache |
Structure to store the cluster list cache. More... | |
struct | Fs_management |
Structure to save the variables frequently used by file system mounted. More... | |
struct | Fs_management_entry |
Structure to save the frequently variables of file system mounted. More... | |
struct | Fs_management_fast |
Structure to save the variables very frequently used by file system mounted. More... | |
union | Fs_rootdir |
Union to define a root directory. More... | |
struct | Fs_sector_cache |
Structure to store the information about sector cache (=last sector read or write on disk) More... | |
struct | Fs_segment |
Structure to define a segment. More... | |
struct | st_fs_cluster |
Structure to store cluster information. More... | |
Macros | |
#define | _GLOBEXT_ extern |
#define | FS_BUF_SECTOR_EMPTY 0xFF |
Signal that sector cache is not valid. More... | |
#define | FS_MBR_OFFSET_PART_ENTRY(num) ((uint16_t)((uint16_t)(0x1BE)+(0x10 * num))) |
Position (unit byte) in the MBR of a partition entry. More... | |
#define | Is_fat12 (FS_TYPE_FAT_12 == fs_g_nav_fast.u8_type_fat) |
#define | Is_fat16 (FS_TYPE_FAT_16 == fs_g_nav_fast.u8_type_fat) |
#define | Is_fat32 (FS_TYPE_FAT_32 == fs_g_nav_fast.u8_type_fat) |
#define | Is_unicode (0) |
Macro to access at fields in BPB sector (only used in fat_mount() function) | |
The name prefixed by "BPB_" are defined in "Hardware White Paper FAT" | |
#define | LOW_16_BPB_BytsPerSec fs_g_sector[11] |
#define | HIGH_16_BPB_BytsPerSec fs_g_sector[12] |
#define | U8_BPB_SecPerClus fs_g_sector[13] |
#define | LOW_16_BPB_RootEntCnt fs_g_sector[17] |
#define | HIGH_16_BPB_RootEntCnt fs_g_sector[18] |
#define | LOW_16_BPB_FATSz16 fs_g_sector[22] |
#define | HIGH_16_BPB_FATSz16 fs_g_sector[23] |
#define | LOW0_32_BPB_FATSz32 fs_g_sector[36] |
#define | LOW1_32_BPB_FATSz32 fs_g_sector[37] |
#define | LOW2_32_BPB_FATSz32 fs_g_sector[38] |
#define | LOW3_32_BPB_FATSz32 fs_g_sector[39] |
#define | LOW_16_BPB_TotSec16 fs_g_sector[19] |
#define | HIGH_16_BPB_TotSec16 fs_g_sector[20] |
#define | LOW0_32_BPB_TotSec32 fs_g_sector[32] |
#define | LOW1_32_BPB_TotSec32 fs_g_sector[33] |
#define | LOW2_32_BPB_TotSec32 fs_g_sector[34] |
#define | LOW3_32_BPB_TotSec32 fs_g_sector[35] |
#define | LOW_16_BPB_ResvSecCnt fs_g_sector[14] |
#define | HIGH_16_BPB_ResvSecCnt fs_g_sector[15] |
#define | U8_BPB_NumFATs fs_g_sector[16] |
#define | LOW0_32_BPB_RootClus fs_g_sector[44] |
#define | LOW1_32_BPB_RootClus fs_g_sector[45] |
#define | LOW2_32_BPB_RootClus fs_g_sector[46] |
#define | LOW3_32_BPB_RootClus fs_g_sector[47] |
#define | LOW_16_BPB_FSInfo fs_g_sector[48] |
#define | HIGH_16_BPB_FSInfo fs_g_sector[49] |
Constants used to sign a MBR or PBR sectors | |
#define | FS_BR_SIGNATURE_LOW 0x55 |
#define | FS_BR_SIGNATURE_HIGH 0xAA |
Constants used in MBR sector | |
#define | FS_PART_BOOTABLE 0x80 |
#define | FS_PART_NO_BOOTABLE 0x00 |
#define | FS_PART_TYPE_FAT12 0x01 |
#define | FS_PART_TYPE_FAT16_INF32M 0x04 |
#define | FS_PART_TYPE_FAT16_SUP32M 0x06 |
#define | FS_PART_TYPE_FAT16_SUP32M_BIS 0x0E |
#define | FS_PART_TYPE_FAT32 0x0B |
#define | FS_PART_TYPE_FAT32_BIS 0x0C |
#define | FS_PART_REMOVE_MEDIA 0xF0 |
#define | FS_PART_NO_REMOVE_MEDIA 0xF8 |
#define | FS_PART_HARD_DISK 0x81 |
#define | FS_BOOT_SIGN 0x29 |
Maximum of FAT cluster | |
#define | FS_FAT12_MAX_CLUSTERS 4085 |
#define | FS_FAT16_MAX_CLUSTERS 65525 |
Constants used in the first byte of file entry | |
#define | FS_ENTRY_END 0x00 |
#define | FS_ENTRY_DEL 0xE5 |
#define | FS_ENTRY_LFN_LAST 0x40 |
Constantes used to manage the file entry | |
#define | FS_SIZE_FILE_ENTRY 32 |
#define | FS_SHIFT_B_TO_FILE_ENTRY 5 |
#define | FS_SIZE_LFN_ENTRY 13 |
#define | FS_SIZE_SFNAME 11 |
#define | FS_SIZE_SFNAME_WITHOUT_EXT 8 |
#define | FS_SIZE_SFNAME_EXT_ONLY 3 |
LIMITATIONS OF FILE SYSTEM | |
#define | FS_NB_FAT 2 |
The unit sector of 512B is many used in file System stack | |
#define | FS_512B 512 |
#define | FS_512B_MASK (512-1) |
#define | FS_512B_SHIFT_BIT 9 |
#define | FS_SIZE_OF_SECTOR FS_512B |
#define | FS_MASK_SIZE_OF_SECTOR FS_512B_MASK |
#define | FS_SHIFT_B_TO_SECTOR FS_512B_SHIFT_BIT |
#define | FS_CACHE_SIZE 512 |
Status of the fat_checkcluster() function | |
#define | FS_CLUS_OK 0 |
#define | FS_CLUS_BAD 1 |
#define | FS_CLUS_END 2 |
Options of the fat_cluster_list() function | |
#define | FS_CLUST_ACT_SEG 0x01 |
#define | FS_CLUST_ACT_ONE 0x02 |
#define | FS_CLUST_ACT_CLR 0x03 |
Options of the fat_cluster_val() function | |
#define | FS_CLUST_VAL_READ false |
#define | FS_CLUST_VAL_WRITE true |
#define | FS_CLUST_VAL_EOL 0x0FFFFFFF |
FAT type ID, used in "Fs_management_fast.u8_type_fat" | |
#define | FS_TYPE_FAT_UNM 0 |
Partition not mounted. More... | |
#define | FS_TYPE_FAT_12 1 |
#define | FS_TYPE_FAT_16 2 |
#define | FS_TYPE_FAT_32 3 |
Value used in "Fs_management_fast.u16_entry_pos_sel_file" | |
#define | FS_NO_SEL 0xFFFF |
Signal that a file entry isn't selected. More... | |
#define | FS_END_FIND 0xFFFE |
Signal that a file entry is the last file entry accessible by system. More... | |
Macro to check the file open mode | |
#define | Fat_file_is_open() (fs_g_nav_entry.u8_open_mode !=0 ) |
#define | Fat_file_isnot_open() (fs_g_nav_entry.u8_open_mode ==0 ) |
#define | Fat_file_close() (fs_g_nav_entry.u8_open_mode =0 ) |
Typedefs | |
Main structures | |
typedef struct st_fs_cluster | Fs_cluster |
Structure to store cluster information. More... | |
Functions | |
bool | fat_format (uint8_t u8_fat_type) |
This function formats the drive. More... | |
uint8_t | fat_get_nbpartition (void) |
This function returns the number of partition present on selected drive. More... | |
bool | fat_mount (void) |
This function mounts a partition. More... | |
bool | fat_serialnumber (bool b_action, uint8_t _MEM_TYPE_SLOW_ *a_u8_sn) |
This function reads or writes a serial number. More... | |
Functions to verify navigator state | |
}@ | |
bool | fat_check_device (void) |
This function checks device state. More... | |
bool | fat_check_mount (void) |
This function checks if the partition is mounted. More... | |
bool | fat_check_noopen (void) |
This function checks if a file is not opened on current navigator. More... | |
bool | fat_check_open (void) |
This function checks if a file is opened on current navigator. More... | |
bool | fat_check_select (void) |
This function checks if a file is selected on current navigator. More... | |
bool | fat_check_mount_noopen (void) |
This function checks if the partition is mounted and no file is opened. More... | |
bool | fat_check_mount_select_noopen (void) |
This function checks if the partition is mounted and if no file is opened and a file is selected. More... | |
bool | fat_check_mount_select_open (void) |
This function checks if the partition is mounted and if a file is opened. More... | |
bool | fat_check_mount_select (void) |
This function checks if the partition is mounted and if a file is selected. More... | |
bool | fat_check_is_file (void) |
This function checks if the selected file entry is a file and not a directory. More... | |
Functions to compute free space on a partition | |
uint32_t | fat_getfreespace (void) |
This function returns the space free in the partition. More... | |
uint8_t | fat_getfreespace_percent (void) |
This function returns the space free in percent. More... | |
bool | fat_write_fat32_FSInfo (uint32_t u32_nb_free_cluster) |
This function writes the space free number in selected FAT32 partition. More... | |
uint32_t | fat_read_fat32_FSInfo (void) |
This function returns the space free in the selected FAT32 partition. More... | |
Functions to manage the cluster list | |
bool | fat_cluster_list (uint8_t opt_action, bool b_for_file) |
This function gets or clears a cluster list. More... | |
void | fat_cache_clusterlist_reset (void) |
This function resets the cluster list caches. More... | |
bool | fat_cluster_val (bool b_mode) |
This function returns or modifies a cluster value in FAT. More... | |
bool | fat_cluster_readnext (void) |
This function is optimized to read a continue cluster list on FAT16 and FAT32. More... | |
uint8_t | fat_checkcluster (void) |
This function checks the cluster value. More... | |
bool | fat_allocfreespace (void) |
This function allocs a cluster list. More... | |
void | fat_clear_info_fat_mod (void) |
This function clears the cache information about FAT modifications. More... | |
bool | fat_clear_cluster (void) |
This function clears one cluster. More... | |
bool | fat_update_fat2 (void) |
This function copies the modifications of the first FAT to the second FAT. More... | |
Functions to read or to write a file or a directory | |
bool | fat_read_file (uint8_t mode) |
This function gets or clears a cluster list at the current position in the selected file. More... | |
bool | fat_write_file (uint8_t mode, uint32_t u32_nb_sector_write) |
This function gets and eventually allocs a cluster list at the current position in the selected file. More... | |
bool | fat_read_dir (void) |
This function fill the internal cache with a sector from current directory. More... | |
bool | fat_initialize_dir (void) |
This function writes the directory information. More... | |
Functions to manage the entry field (fat.c) | |
bool | fat_entry_check (bool b_type) |
This function checks the entry. More... | |
bool | fat_entry_checkext (FS_STRING sz_filter) |
This function checks the file extension. More... | |
void | fat_get_entry_info (void) |
This function reads information about selected file. More... | |
bool | fat_entry_is_dir (void) |
This function checks if the entry file is a directory. More... | |
void | fat_clear_entry_info_and_ptr (void) |
This function resets the selection pointers. More... | |
void | fat_write_entry_file (void) |
This function writes the information about selected file. More... | |
bool | fat_entry_shortname (FS_STRING sz_name, uint8_t u8_size_max, bool b_mode) |
This function returns or compares the short name entry. More... | |
bool | fat_entry_longname (FS_STRING sz_name, uint8_t u8_size_max, bool b_mode, bool b_match_case) |
This function returns or compares the long name entry. More... | |
bool | fat_check_eof_name (uint16_t character) |
Check end of name. More... | |
PTR_CACHE | fat_get_ptr_entry (void) |
This function returns a cache pointer on the current entry. More... | |
Functions to manage the entry field (fat_unusual.c) | |
bool | fat_create_entry_file_name (FS_STRING sz_name) |
This function creates the short and the long name of a new entry. More... | |
void | fat_get_date (FS_STRING sz_date, bool type_date) |
This function reads the information about a date. More... | |
void | fat_set_date (const FS_STRING sz_date, bool type_date) |
This function changes the date information. More... | |
bool | fat_delete_file (bool b_cluster_list) |
This function deletes the file entries and cluster list. More... | |
bool | fat_entry_label (bool b_action, FS_STRING sz_label) |
This function reads or writes a label in the partition. More... | |
Functions to manage the cache | |
bool | fat_cache_read_sector (bool b_load) |
This function loads a memory sector in internal cache sector. More... | |
void | fat_cache_reset (void) |
This function resets the sector cache. More... | |
void | fat_cache_clear (void) |
This function clears the sector cache. More... | |
void | fat_cache_mark_sector_as_dirty (void) |
This function sets a flag to signal that sector cache is modified. More... | |
bool | fat_cache_flush (void) |
This function flushes the sector cache on the memory if necessary. More... | |
Functions to control access disk | |
bool | fat_check_nav_access_disk (void) |
This function checks write access. More... | |
bool | fat_check_nav_access_file (bool mode) |
This function checks all access at current file. More... | |
Functions to manage navigator switch | |
void | fat_invert_nav (uint8_t u8_idnav) |
This function inverts the current navigation with another. More... | |
void | fat_copy_nav (uint8_t u8_idnav) |
This function copies the main navigator to another navigator. More... | |
Variables | |
_GLOBEXT_ _MEM_TYPE_FAST_ Fs_cluster | fs_g_cluster |
To take time in functions: fat_getfreespace, fat_cluster_list, fat_cluster_val, fat_checkcluster. More... | |
_GLOBEXT_ _MEM_TYPE_FAST_ Fs_segment | fs_g_seg |
Variable frequently used by many function (optimization, no parameter in function) More... | |
_GLOBEXT_ bool | g_b_no_check_disk |
Variables to enable/disable the disk check before each action on disk. More... | |
_GLOBEXT_ bool | g_b_string_length |
Variables to select LENGTH string mode (initialised in nav_reset()) More... | |
_GLOBEXT_ bool | g_b_unicode |
Variables to select string format (initialised in nav_reset()) More... | |
Variables initialized in drive_mount() | |
_GLOBEXT_ _MEM_TYPE_SLOW_ Fs_management | fs_g_nav |
_GLOBEXT_ _MEM_TYPE_FAST_ Fs_management_fast | fs_g_nav_fast |
_GLOBEXT_ _MEM_TYPE_SLOW_ Fs_management_entry | fs_g_nav_entry |
Variables used to update the second FAT zone | |
_GLOBEXT_ _MEM_TYPE_SLOW_ uint32_t | fs_g_u32_first_mod_fat |
Offset (unit 512B) in fat of the first sector (unit 512B) More... | |
_GLOBEXT_ _MEM_TYPE_SLOW_ uint32_t | fs_g_u32_last_mod_fat |
Offset (unit 512B) in fat of the last sector (unit 512B) More... | |
Variables used to manage the sector cache | |
typedef uint8_t _MEM_TYPE_SLOW_ * | PTR_CACHE |
_GLOBEXT_ _MEM_TYPE_SLOW_ uint8_t | fs_g_sector [FS_CACHE_SIZE] |
Use "FAT sector cache" to store a sector from a file (see file_putc(), file_getc(), file_read_buf(), file_write_buf()) More... | |
_GLOBEXT_ _MEM_TYPE_SLOW_ Fs_sector_cache | fs_g_sectorcache |
_GLOBEXT_ _MEM_TYPE_SLOW_ uint32_t | fs_gu32_addrsector |
Store the address of future cache (unit 512B) More... | |