Microchip® Advanced Software Framework

smc.h File Reference

Static Memory Controller (SMC) driver for SAM.

Copyright (c) 2011-2018 Microchip Technology Inc. and its subsidiaries.

#include "compiler.h"

Macros

#define ECC_STATUS_MASK   0x07
 
#define NFC_BUSY_FLAG   0x8000000
 
#define NFCADDR_CMD_ACYCLE   (0x7u << 19) /* Number of Address required for the current command */
 
#define NFCADDR_CMD_ACYCLE_FIVE   (0x5u << 19) /* Five address cycles */
 
#define NFCADDR_CMD_ACYCLE_FOUR   (0x4u << 19) /* Four address cycles */
 
#define NFCADDR_CMD_ACYCLE_NONE   (0x0u << 19) /* No address cycle */
 
#define NFCADDR_CMD_ACYCLE_ONE   (0x1u << 19) /* One address cycle */
 
#define NFCADDR_CMD_ACYCLE_THREE   (0x3u << 19) /* Three address cycles */
 
#define NFCADDR_CMD_ACYCLE_TWO   (0x2u << 19) /* Two address cycles */
 
#define NFCADDR_CMD_CMD1   (0xFFu << 2) /* Command Register Value for Cycle 1 */
 
#define NFCADDR_CMD_CMD2   (0xFFu << 10) /* Command Register Value for Cycle 2 */
 
#define NFCADDR_CMD_CSID(value)   ((NFCADDR_CMD_CSID_Msk & ((value) << NFCADDR_CMD_CSID_Pos)))
 
#define NFCADDR_CMD_CSID_Msk   (0x7u << NFCADDR_CMD_CSID_Pos) /* Chip Select Identifier */
 
#define NFCADDR_CMD_CSID_Pos   22
 
#define NFCADDR_CMD_NFC_READ   (0x0u << 26) /* NFC Write Enable */
 
#define NFCADDR_CMD_NFC_WIRTE   (0x1u << 26) /* NFC Write Enable */
 
#define NFCADDR_CMD_NFCCMD   (0x1u << 27) /* NFC Command Enable */
 
#define NFCADDR_CMD_NFCEN   (0x1u << 25) /* NFC Enable */
 
#define NFCADDR_CMD_VCMD2   (0x1u << 18) /* Valid Cycle 2 Command */
 

Functions

uint32_t smc_ecc_get_status (Smc *p_smc, uint32_t ul_parity_number)
 
void smc_ecc_get_value (Smc *p_smc, uint32_t *p_ecc)
 
void smc_ecc_init (Smc *p_smc, uint32_t ul_type, uint32_t ul_pagesize)
 
void smc_enable_writeprotect (Smc *p_smc, uint32_t ul_enable)
 
uint32_t smc_get_mode (Smc *p_smc, uint32_t ul_cs)
 
uint32_t smc_get_writeprotect_status (Smc *p_smc)
 
void smc_nfc_disable (Smc *p_smc)
 
void smc_nfc_disable_interrupt (Smc *p_smc, uint32_t ul_sources)
 
void smc_nfc_disable_spare_read (Smc *p_smc)
 
void smc_nfc_disable_spare_write (Smc *p_smc)
 
void smc_nfc_enable (Smc *p_smc)
 
void smc_nfc_enable_interrupt (Smc *p_smc, uint32_t ul_sources)
 
void smc_nfc_enable_spare_read (Smc *p_smc)
 
void smc_nfc_enable_spare_write (Smc *p_smc)
 
uint32_t smc_nfc_get_interrupt_mask (Smc *p_smc)
 
uint32_t smc_nfc_get_status (Smc *p_smc)
 
void smc_nfc_init (Smc *p_smc, uint32_t ul_config)
 
void smc_nfc_send_command (Smc *p_smc, uint32_t ul_cmd, uint32_t ul_address_cycle, uint32_t ul_cycle0)
 
void smc_nfc_set_address0 (Smc *p_smc, uint8_t uc_address0)
 
void smc_nfc_set_bank (Smc *p_smc, uint32_t ul_bank)
 
void smc_nfc_set_page_size (Smc *p_smc, uint32_t ul_page_size)
 
void smc_set_cycle_timing (Smc *p_smc, uint32_t ul_cs, uint32_t ul_cycle_timing)
 
void smc_set_mode (Smc *p_smc, uint32_t ul_cs, uint32_t ul_mode)
 
void smc_set_nand_timing (Smc *p_smc, uint32_t ul_cs, uint32_t ul_nand_timing)
 
void smc_set_pulse_timing (Smc *p_smc, uint32_t ul_cs, uint32_t ul_pulse_timing)
 
void smc_set_setup_timing (Smc *p_smc, uint32_t ul_cs, uint32_t ul_setup_timing)