task.
h
void vTaskResume( xTaskHandle pxTaskToResume );
INCLUDE_vTaskSuspend must be defined as 1 for this function to be available. See the configuration section for more information.
Resumes a suspended task.
A task that has been suspended by one of more calls to vTaskSuspend () will be made available for running again by a single call to vTaskResume ().
pxTaskToResume | Handle to the task being readied. |
Example usage:
void vAFunction( void ) { xTaskHandle xHandle;
Create a task, storing the handle. xTaskCreate( vTaskCode, "NAME", STACK_SIZE, NULL, tskIDLE_PRIORITY, &xHandle );
...
Use the handle to suspend the created task. vTaskSuspend( xHandle );
...
The created task will not run during this period, unless another task calls vTaskResume( xHandle ).
...
Resume the suspended task ourselves. vTaskResume( xHandle );
The created task will once again get microcontroller processing time in accordance with it priority within the system. }