Microchip® Advanced Software Framework

tstrEthInitParam Struct Reference

Structure to hold ethernet interface parameters.

Structure is to be defined and have its attributes set,based on the application's functiality before 
a call is made to the initialize the wi-fi operations by calling the  @ref m2m_wifi_init function.
Part of the wi-fi configuration structure @ref tstrWifiInitParam.
See Also
tpfAppEthCb tpfAppWifiCb m2m_wifi_init

#include <m2m_wifi.h>

Data Fields

uint8au8ethRcvBuf
 
tpfAppEthCb pfAppEthCb
 
uint16 u16ethRcvBufSize