Type by which tasks are referenced. For example, a call to xTaskCreate returns (via a pointer parameter) an xTaskHandle variable that can then be used as a parameter to vTaskDelete to delete the task.
Generated on Sat Mar 5 2022 00:39:24 for WILC1000/WILC3000 Weather WiFi Concurrent Mode and Bluetooth Demo for SAM4S XPlained Pro by 1.8.5