Below is a table listing the acronyms used in this module, along with their intended meanings.
Acronym | Definition |
---|---|
AHB | Advanced High-performance Bus |
AMBA | Advanced Microcontroller Bus Architecture |
QSG | Quick Start Guide |
RCR | Receive Counter Register |
RNCR | Return Receive Next Counter Register |
RNPR | Receive Next Pointer Register |
RPR | Receive Pointer Register |
TCR | Transmit Counter Register |
TNCR | Transmit Next Counter Register |
TNPR | Transmit Next Pointer Register |
TPR | Transmit Pointer Register |
This driver has the following dependencies:
There are no errata related to this driver.
An overview of the module history is presented in the table below, with details on the enhancements and fixes made to the module since its first release. The current version of this corresponds to the newest version in the table.
Changelog |
---|
Initial document release |