Type by which tasks are referenced. For example, a call to xTaskCreate returns (via a pointer parameter) an xTaskHandle variable that can then be used as a parameter to vTaskDelete to delete the task.
Generated on Sat Mar 5 2022 00:41:14 for WINC3400 Mode STA ByPass Example - SAM4S XPlained Pro by 1.8.5