CPU reset cause functions.
Copyright (c) 2010-2018 Microchip Technology Inc. and its subsidiaries.
Macros | |
#define | CHIP_RESET_CAUSE_CPU_ERROR 0 |
CPU error reset cause not available on this chip. More... | |
#define | CHIP_RESET_CAUSE_JTAG 0 |
JTAG reset cause not available on this chip. More... | |
#define | CHIP_RESET_CAUSE_POR_IO 0 |
Power-on-reset on I/O power domain reset cause not available on this chip. More... | |
#define | CHIP_RESET_CAUSE_SLEEP 0 |
Wake from Shutdown sleep mode reset cause not available on this chip. More... | |
Enumerations | |
enum | reset_cause { RESET_CAUSE_BOD_CPU = CHIP_RESET_CAUSE_BOD_CPU, RESET_CAUSE_BOD_IO = CHIP_RESET_CAUSE_BOD_IO, RESET_CAUSE_CPU_ERROR = CHIP_RESET_CAUSE_CPU_ERROR, RESET_CAUSE_EXTRST = CHIP_RESET_CAUSE_EXTRST, RESET_CAUSE_JTAG = CHIP_RESET_CAUSE_JTAG, RESET_CAUSE_OCD = CHIP_RESET_CAUSE_OCD, RESET_CAUSE_POR = CHIP_RESET_CAUSE_POR, RESET_CAUSE_POR_IO = CHIP_RESET_CAUSE_POR_IO, RESET_CAUSE_SLEEP = CHIP_RESET_CAUSE_SLEEP, RESET_CAUSE_SOFT = CHIP_RESET_CAUSE_SOFT, RESET_CAUSE_SPIKE = CHIP_RESET_CAUSE_SPIKE, RESET_CAUSE_WDT = CHIP_RESET_CAUSE_WDT } |
List of reset causes in bit-mask format. More... | |
Functions | |
Specific reset cause helper functions | |
static bool | reset_cause_is_cpu_brown_out_detected (void) |
Check if chip reset was caused by a CPU power brown-out detection. More... | |
static bool | reset_cause_is_io_brown_out_detected (void) |
Check if chip reset was caused by an I/O power brown-out detection. More... | |
static bool | reset_cause_is_brown_out_detected (void) |
Check if chip reset was caused by a brown-out detection on any power domain. More... | |
static bool | reset_cause_is_cpu_error (void) |
Check if chip reset was caused by a CPU error, illegal access. More... | |
static bool | reset_cause_is_external_reset (void) |
Check if chip reset was caused by an external reset. More... | |
static bool | reset_cause_is_jtag (void) |
Check if chip reset was caused by a JTAG reset. More... | |
static bool | reset_cause_is_ocd (void) |
Check if chip reset was caused by the on-chip debug system. More... | |
static bool | reset_cause_is_power_on_reset (void) |
Check if chip reset was caused by a power-on-reset. More... | |
static bool | reset_cause_is_io_power_on_reset (void) |
Check if chip reset was caused by an I/O power-on-reset. More... | |
static bool | reset_cause_is_wake_from_shutdown_sleep (void) |
Check if chip reset was caused by a wake up from shutdown sleep mode. More... | |
static bool | reset_cause_is_software_reset (void) |
Check if chip reset was caused by a software reset. More... | |
static bool | reset_cause_is_spike_detected (void) |
Check if chip reset was caused by a power spike detection. More... | |
static bool | reset_cause_is_watchdog (void) |
Check if chip reset was caused by a watchdog timeout. More... | |