Type by which tasks are referenced. For example, a call to xTaskCreate returns (via a pointer parameter) an TaskHandle_t variable that can then be used as a parameter to vTaskDelete to delete the task.
Generated on Fri Mar 4 2022 23:25:02 for FreeRTOS demo using event group feature on OLED1 Xplained Pro, for SAM D21 Xplained Pro by 1.8.5