Microchip® Advanced Software Framework

freertos_peripheral_control.h File Reference

FreeRTOS Peripheral Control API Functions.

Copyright (c) 2012-2018 Microchip Technology Inc. and its subsidiaries.

#include <conf_board.h>
#include "status_codes.h"
#include "pdc.h"
#include "FreeRTOS.h"
#include "semphr.h"

Data Structures

struct  freertos_peripheral_options
 Define the behaviour of FreeRTOS ASF read and write functions for a peripheral. More...
 

Macros

#define USE_RX_ACCESS_MUTEX   0x02
 Bit definition used in the options_flags member of a freertos_peripheral_options_t structure passed as a parameter to an initialization function to indicate that reads from the peripheral being initialized must be thread aware. More...
 
#define USE_TX_ACCESS_SEM   0x01
 Bit definition used in the options_flags member of a freertos_peripheral_options_t structure passed as a parameter to an initialization function to indicate that writes to the peripheral being initialized must be thread aware. More...
 
#define WAIT_RX_COMPLETE   0x08
 Bit definition used in the options_flags member of a freertos_peripheral_options_t structure passed as a parameter to an initialization function to indicate that a task reading from the peripheral must be held in the FreeRTOS Blocked state until the read has completed. More...
 
#define WAIT_TX_COMPLETE   0x04
 Bit definition used in the options_flags member of a freertos_peripheral_options_t structure passed as a parameter to an initialization function to indicate that a task writing to the peripheral must be held in the FreeRTOS Blocked state until the write has completed. More...
 

Typedefs

typedef struct
freertos_peripheral_options 
freertos_peripheral_options_t
 Define the behaviour of FreeRTOS ASF read and write functions for a peripheral. More...
 

Enumerations

enum  peripheral_operation_mode {
  USART_RS232 = 0,
  UART_RS232,
  SPI_MASTER,
  TWI_I2C_MASTER,
  TWIHS_I2C_MASTER,
  NOT_SUPPORTED
}
 Defines the operating modes that can be specified in a freertos_peripheral_options_t structure. More...