Type by which tasks are referenced. For example, a call to xTaskCreate returns (via a pointer parameter) an TaskHandle_t variable that can then be used as a parameter to vTaskDelete to delete the task.
Generated on Sat Mar 5 2022 00:35:07 for Peripheral Control FreeRTOS Example for SAM4S Xplained by 1.8.5