Type by which tasks are referenced. For example, a call to xTaskCreate returns (via a pointer parameter) an TaskHandle_t variable that can then be used as a parameter to vTaskDelete to delete the task.
Generated on Sat Mar 5 2022 00:31:38 for Basic FreeRTOS Example for SAM4S-EK2 by 1.8.5