Microchip® Advanced Software Framework

•All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
vTaskSuspend

task.

h

void vTaskSuspend( TaskHandle_t xTaskToSuspend );

INCLUDE_vTaskSuspend must be defined as 1 for this function to be available. See the configuration section for more information.

Suspend any task. When suspended a task will never get any microcontroller processing time, no matter what its priority.

Calls to vTaskSuspend are not accumulative - i.e. calling vTaskSuspend () twice on the same task still only requires one call to vTaskResume () to ready the suspended task.

Parameters
xTaskToSuspendHandle to the task being suspended. Passing a NULL handle will cause the calling task to be suspended.

Example usage:

 void vAFunction( void )
 {
 TaskHandle_t xHandle;
Create a task, storing the handle.
     xTaskCreate( vTaskCode, "NAME", STACK_SIZE, NULL, tskIDLE_PRIORITY, &xHandle );
...
Use the handle to suspend the created task.
     vTaskSuspend( xHandle );
...
The created task will not run during this period, unless
another task calls vTaskResume( xHandle ).
...
Suspend ourselves.
     vTaskSuspend( NULL );
We cannot get here unless another task calls vTaskResume
with our handle as the parameter.
 }