task.
h
void vTaskSuspendAll( void );
Suspends the scheduler without disabling interrupts. Context switches will not occur while the scheduler is suspended.
After calling vTaskSuspendAll () the calling task will continue to execute without risk of being swapped out until a call to xTaskResumeAll () has been made.
API functions that have the potential to cause a context switch (for example, vTaskDelayUntil(), xQueueSend(), etc.) must not be called while the scheduler is suspended.
Example usage:
void vTask1( void * pvParameters ) { for( ;; ) { Task code goes here.
...
At some point the task wants to perform a long operation during which it does not want to get swapped out. It cannot use taskENTER_CRITICAL ()/taskEXIT_CRITICAL () as the length of the operation may cause interrupts to be missed - including the ticks.
Prevent the real time kernel swapping out the task. vTaskSuspendAll ();
Perform the operation here. There is no need to use critical sections as we have all the microcontroller processing time. During this time interrupts will still operate and the kernel tick count will be maintained.
...
The operation is complete. Restart the kernel. xTaskResumeAll (); } }