|
static void | ili9488_check_box_coordinates (uint32_t *p_ul_x1, uint32_t *p_ul_y1, uint32_t *p_ul_x2, uint32_t *p_ul_y2) |
| Check box coordinates. More...
|
|
void | ili9488_copy_pixels_from_screen (uint16_t *pixels, uint32_t count) |
| Copy pixels from the screen to a pixel buffer. More...
|
|
void | ili9488_copy_pixels_to_screen (const uint16_t *pixels, uint32_t count) |
| Copy pixels from SRAM to the screen. More...
|
|
void | ili9488_delay (uint32_t ul_ms) |
| Delay function. More...
|
|
void | ili9488_display_off (void) |
| Turn off the LCD. More...
|
|
void | ili9488_display_on (void) |
| Turn on the LCD. More...
|
|
static void | ili9488_draw_char (uint32_t ul_x, uint32_t ul_y, uint8_t uc_c) |
| Draw an ASCII character on LCD. More...
|
|
uint32_t | ili9488_draw_circle (uint32_t ul_x, uint32_t ul_y, uint32_t ul_r) |
| Draw a circle on LCD. More...
|
|
uint32_t | ili9488_draw_filled_circle (uint32_t ul_x, uint32_t ul_y, uint32_t ul_r) |
| Draw a filled circle on LCD. More...
|
|
void | ili9488_draw_filled_rectangle (uint32_t ul_x1, uint32_t ul_y1, uint32_t ul_x2, uint32_t ul_y2) |
| Draw a filled rectangle on LCD. More...
|
|
void | ili9488_draw_line (uint32_t ul_x1, uint32_t ul_y1, uint32_t ul_x2, uint32_t ul_y2) |
| Draw a line on LCD. More...
|
|
static void | ili9488_draw_line_bresenham (uint32_t ul_x1, uint32_t ul_y1, uint32_t ul_x2, uint32_t ul_y2) |
| Draw a line on LCD, which is not horizontal or vertical. More...
|
|
uint32_t | ili9488_draw_pixel (uint32_t ul_x, uint32_t ul_y) |
| Draw a pixel on LCD. More...
|
|
void | ili9488_draw_pixmap (uint32_t ul_x, uint32_t ul_y, uint32_t ul_width, uint32_t ul_height, const ili9488_color_t *p_ul_pixmap) |
| Draw a pixmap on LCD. More...
|
|
void | ili9488_draw_prepare (uint32_t ul_x, uint32_t ul_y, uint32_t ul_width, uint32_t ul_height) |
| Prepare LCD to draw. More...
|
|
void | ili9488_draw_rectangle (uint32_t ul_x1, uint32_t ul_y1, uint32_t ul_x2, uint32_t ul_y2) |
| Draw a rectangle on LCD. More...
|
|
void | ili9488_draw_string (uint32_t ul_x, uint32_t ul_y, const uint8_t *p_str) |
| Draw a string on LCD. More...
|
|
void | ili9488_duplicate_pixel (const uint16_t color, uint32_t count) |
| Set a given number of pixels to the same color. More...
|
|
void | ili9488_fill (ili9488_color_t ul_color) |
| Fill the LCD buffer with the specified color. More...
|
|
ili9488_color_t | ili9488_get_pixel (uint32_t ul_x, uint32_t ul_y) |
| Get a pixel from LCD. More...
|
|
uint32_t | ili9488_init (struct ili9488_opt_t *p_opt) |
| Initialize the ILI9488 lcd driver. More...
|
|
static uint32_t | ili9488_lcd_get_16 (void) |
| Read 32 bit data. More...
|
|
static uint32_t | ili9488_read_chipid (void) |
| Read chipid. More...
|
|
uint16_t | ili9488_read_gram (void) |
| Read a single color from the graphical memory. More...
|
|
static uint32_t | ili9488_read_ram (void) |
| Read data to LCD GRAM. More...
|
|
void | ili9488_scroll (uint16_t ul_tfa, uint16_t ul_vsa, uint16_t ul_bfa) |
| Scroll up/down for the number of specified lines. More...
|
|
void | ili9488_set_bottom_right_limit (ili9488_coord_t x, ili9488_coord_t y) |
| Set the display bottom right drawing limit. More...
|
|
void | ili9488_set_cursor_position (uint16_t x, uint16_t y) |
| Set cursor of LCD screen. More...
|
|
void | ili9488_set_display_direction (enum ili9488_display_direction direction) |
| ILI9488 configure landscape. More...
|
|
void | ili9488_set_foreground_color (uint32_t ul_color) |
| Set foreground color. More...
|
|
void | ili9488_set_limits (ili9488_coord_t start_x, ili9488_coord_t start_y, ili9488_coord_t end_x, ili9488_coord_t end_y) |
| Set the full display drawing limits. More...
|
|
void | ili9488_set_orientation (uint8_t flags) |
| Sets the orientation of the display data. More...
|
|
void | ili9488_set_scroll_address (uint16_t ul_vsp) |
| Enable the scrolling feature. More...
|
|
void | ili9488_set_top_left_limit (ili9488_coord_t x, ili9488_coord_t y) |
| Set the display top left drawing limit. More...
|
|
void | ili9488_set_window (uint16_t x, uint16_t y, uint16_t width, uint16_t height) |
| ILI9488 configure window. More...
|
|
void | ili9488_write_brightness (uint16_t us_value) |
| Set display brightness. More...
|
|
void | ili9488_write_gram (uint16_t color) |
| Write the graphical memory with a single color pixel. More...
|
|
static void | ili9488_write_ram (ili9488_color_t ul_color) |
| Write data to LCD GRAM. More...
|
|
static void | ili9488_write_ram_buffer (const ili9488_color_t *p_ul_buf, uint32_t ul_size) |
| Write multiple data in buffer to LCD controller. More...
|
|
static void | ili9488_write_ram_prepare (void) |
| Prepare to write GRAM data. More...
|
|
static void | ili9488_write_register (uint8_t uc_reg, const ili9488_color_t *us_data, uint32_t size) |
| Write data to LCD Register. More...
|
|