Microchip® Advanced Software Framework

udi_hid_mouse.h File Reference

USB Device Human Interface Device (HID) mouse interface.

Copyright (c) 2009-2018 Microchip Technology Inc. and its subsidiaries.

#include "conf_usb.h"
#include "usb_protocol.h"
#include "usb_protocol_hid.h"
#include "udc_desc.h"
#include "udi.h"

Data Structures

struct  udi_hid_mouse_desc_t
 Interface descriptor structure for HID mouse. More...
 
struct  udi_hid_mouse_report_desc_t
 Report descriptor for HID mouse. More...
 

Macros

#define UDI_HID_MOUSE_DESC
 Content of HID mouse interface descriptor for all speed. More...
 
#define UDI_HID_MOUSE_EP_SIZE   8
 By default no string associated to this interface. More...
 

Functions

Interfaces for mouse events
bool udi_hid_mouse_moveScroll (int8_t pos)
 Move the scroll wheel. More...
 
bool udi_hid_mouse_moveY (int8_t pos_y)
 Move the mouse pointer on Y axe. More...
 
bool udi_hid_mouse_moveX (int8_t pos_x)
 Move the mouse pointer on X axe. More...
 

Variables

UDC_DESC_STORAGE udi_api_t udi_api_hid_mouse
 Global structure which contains standard UDI API for UDC. More...
 

Interfaces for buttons events

#define HID_MOUSE_BTN_DOWN   true
 Value to signal a button down (pressed) More...
 
#define HID_MOUSE_BTN_UP   false
 Value to signal a button up (released) More...
 
bool udi_hid_mouse_btnmiddle (bool b_state)
 Changes middle button state. More...
 
bool udi_hid_mouse_btnright (bool b_state)
 Changes right button state. More...
 
bool udi_hid_mouse_btnleft (bool b_state)
 Changes left button state. More...