Type by which tasks are referenced. For example, a call to xTaskCreate returns (via a pointer parameter) an TaskHandle_t variable that can then be used as a parameter to vTaskDelete to delete the task.
Generated on Sat Mar 5 2022 00:02:04 for USB Device Mass Storage for SAME70-Xplained with FreeRTOS by 1.8.5