In this use case, the USB serial strings is dynamic.
For a static serial string refer to Use USB strings.
Setup steps
Prior to implement this use case, be sure to have already apply the UDI module "basic use case".
Usage steps
Example code
Content of conf_usb.h:
#define USB_DEVICE_SERIAL_NAME
#define USB_DEVICE_GET_SERIAL_NAME_POINTER serial_number
#define USB_DEVICE_GET_SERIAL_NAME_LENGTH 12
extern uint8_t serial_number[];
Add to application C-file:
uint8_t serial_number[USB_DEVICE_GET_SERIAL_NAME_LENGTH];
void init_build_usb_serial_number(void)
{
serial_number[0] = 'A';
serial_number[1] = 'B';
...
serial_number[USB_DEVICE_GET_SERIAL_NAME_LENGTH-1] = 'C';
}
Workflow
- Ensure that conf_usb.h is available and contains the following parameters required to enable a USB serial number strings dynamically:
#define USB_DEVICE_SERIAL_NAME // Define this empty
#define USB_DEVICE_GET_SERIAL_NAME_POINTER serial_number // Give serial array pointer
#define USB_DEVICE_GET_SERIAL_NAME_LENGTH 12 // Give size of serial array
extern uint8_t serial_number[]; // Declare external serial array
- Before start USB stack, initialize the serial array
uint8_t serial_number[USB_DEVICE_GET_SERIAL_NAME_LENGTH];
void init_build_usb_serial_number(void)
{
serial_number[0] = 'A';
serial_number[1] = 'B';
...
serial_number[USB_DEVICE_GET_SERIAL_NAME_LENGTH-1] = 'C';
}