Static Memory Controller (SMC) driver for SAM.
Copyright (c) 2011-2018 Microchip Technology Inc. and its subsidiaries.
#include "compiler.h"
Macros | |
#define | ECC_STATUS_MASK 0x07 |
#define | NFC_BUSY_FLAG 0x8000000 |
#define | NFCADDR_CMD_ACYCLE (0x7u << 19) /* Number of Address required for the current command */ |
#define | NFCADDR_CMD_ACYCLE_FIVE (0x5u << 19) /* Five address cycles */ |
#define | NFCADDR_CMD_ACYCLE_FOUR (0x4u << 19) /* Four address cycles */ |
#define | NFCADDR_CMD_ACYCLE_NONE (0x0u << 19) /* No address cycle */ |
#define | NFCADDR_CMD_ACYCLE_ONE (0x1u << 19) /* One address cycle */ |
#define | NFCADDR_CMD_ACYCLE_THREE (0x3u << 19) /* Three address cycles */ |
#define | NFCADDR_CMD_ACYCLE_TWO (0x2u << 19) /* Two address cycles */ |
#define | NFCADDR_CMD_CMD1 (0xFFu << 2) /* Command Register Value for Cycle 1 */ |
#define | NFCADDR_CMD_CMD2 (0xFFu << 10) /* Command Register Value for Cycle 2 */ |
#define | NFCADDR_CMD_CSID(value) ((NFCADDR_CMD_CSID_Msk & ((value) << NFCADDR_CMD_CSID_Pos))) |
#define | NFCADDR_CMD_CSID_Msk (0x7u << NFCADDR_CMD_CSID_Pos) /* Chip Select Identifier */ |
#define | NFCADDR_CMD_CSID_Pos 22 |
#define | NFCADDR_CMD_NFC_READ (0x0u << 26) /* NFC Write Enable */ |
#define | NFCADDR_CMD_NFC_WIRTE (0x1u << 26) /* NFC Write Enable */ |
#define | NFCADDR_CMD_NFCCMD (0x1u << 27) /* NFC Command Enable */ |
#define | NFCADDR_CMD_NFCEN (0x1u << 25) /* NFC Enable */ |
#define | NFCADDR_CMD_VCMD2 (0x1u << 18) /* Valid Cycle 2 Command */ |
Functions | |
uint32_t | smc_ecc_get_status (Smc *p_smc, uint32_t ul_parity_number) |
void | smc_ecc_get_value (Smc *p_smc, uint32_t *p_ecc) |
void | smc_ecc_init (Smc *p_smc, uint32_t ul_type, uint32_t ul_pagesize) |
void | smc_enable_writeprotect (Smc *p_smc, uint32_t ul_enable) |
uint32_t | smc_get_mode (Smc *p_smc, uint32_t ul_cs) |
uint32_t | smc_get_writeprotect_status (Smc *p_smc) |
void | smc_nfc_disable (Smc *p_smc) |
void | smc_nfc_disable_interrupt (Smc *p_smc, uint32_t ul_sources) |
void | smc_nfc_disable_spare_read (Smc *p_smc) |
void | smc_nfc_disable_spare_write (Smc *p_smc) |
void | smc_nfc_enable (Smc *p_smc) |
void | smc_nfc_enable_interrupt (Smc *p_smc, uint32_t ul_sources) |
void | smc_nfc_enable_spare_read (Smc *p_smc) |
void | smc_nfc_enable_spare_write (Smc *p_smc) |
uint32_t | smc_nfc_get_interrupt_mask (Smc *p_smc) |
uint32_t | smc_nfc_get_status (Smc *p_smc) |
void | smc_nfc_init (Smc *p_smc, uint32_t ul_config) |
void | smc_nfc_send_command (Smc *p_smc, uint32_t ul_cmd, uint32_t ul_address_cycle, uint32_t ul_cycle0) |
void | smc_nfc_set_address0 (Smc *p_smc, uint8_t uc_address0) |
void | smc_nfc_set_bank (Smc *p_smc, uint32_t ul_bank) |
void | smc_nfc_set_page_size (Smc *p_smc, uint32_t ul_page_size) |
void | smc_set_cycle_timing (Smc *p_smc, uint32_t ul_cs, uint32_t ul_cycle_timing) |
void | smc_set_mode (Smc *p_smc, uint32_t ul_cs, uint32_t ul_mode) |
void | smc_set_nand_timing (Smc *p_smc, uint32_t ul_cs, uint32_t ul_nand_timing) |
void | smc_set_pulse_timing (Smc *p_smc, uint32_t ul_cs, uint32_t ul_pulse_timing) |
void | smc_set_setup_timing (Smc *p_smc, uint32_t ul_cs, uint32_t ul_setup_timing) |