- Group External oscillator
- Need to measure the actual startup time on the hardware.
- Group External oscillator
- Need to measure the actual startup time on the hardware.
- Global font_data_type
- Add support for fonts in regular ram
- Global pll_wait_for_lock (unsigned int pll_id)
- Use a timeout to avoid waiting forever and hanging the system
- Global sysclk_get_main_hz (void)
- This function assumes that the main clock source never changes once it's been set up, and that PLL0 always runs at the compile-time configured default rate. While this is probably the most common configuration, which we want to support as a special case for performance reasons, we will at some point need to support more dynamic setups as well.