Microchip® Advanced Software Framework

Todo List
Global app_widget_launch (void)

Add code to set up button here.

Add code to set up basic frame here.

Global app_widget_launch (void)

Add code to set up button here.

Add code to set up basic frame here.

Global font_data_type
Add support for fonts in regular ram
Global pll_wait_for_lock (unsigned int pll_id)
Use a timeout to avoid waiting forever and hanging the system
Global sub_frame_draw_handler (struct win_window *win, struct win_clip_region const *clip)
Add code here to draw text on screen using the gfx_draw_string() function.
Global sysclk_get_main_hz (void)
This function assumes that the main clock source never changes once it's been set up, and that PLL0 always runs at the compile-time configured default rate. While this is probably the most common configuration, which we want to support as a special case for performance reasons, we will at some point need to support more dynamic setups as well.
Global widget_frame_command_handler (struct wtk_basic_frame *frame, win_command_t command_data)
Add code here to handle button press.