Microchip® Advanced Software Framework

stdio_serial.h File Reference

Common Standard I/O Serial Management.

This file defines a useful set of functions for the Stdio Serial interface on SAM0 devices.

Copyright (c) 2009-2018 Microchip Technology Inc. and its subsidiaries.

#include <serial.h>
#include <stdio.h>

Variables

void(* ptr_get )(void volatile *, char *)
 Pointer to the external low level read function. More...
 
int(* ptr_put )(void volatile *, char)
 Pointer to the external low level write function. More...
 
volatile void *volatile stdio_base
 Pointer to the base of the USART module instance to use for stdio. More...