WINC Application Interface Internal Types.
Copyright (c) 2017-2021 Microchip Technology Inc. and its subsidiaries.
#include "common/include/nm_common.h"
#include "driver/include/m2m_types.h"
#include "driver/source/nmdrv.h"
#include "ecc_types.h"
#include "socket/include/socket.h"
Typedefs | |
typedef void(* | tpfAppSSLCb )(uint8 u8MsgType, void *pvMsg) |
A callback to get SSL notifications. More... | |
Functions | |
NMI_API void | m2m_ssl_ecc_process_done (void) |
Allow SSL driver to tidy up after application has finished processing ECC message. More... | |
NMI_API sint8 | m2m_ssl_handshake_rsp (tstrEccReqInfo *strECCResp, uint8 *pu8RspDataBuff, uint16 u16RspDataSz) |
Sends ECC responses to the WINC. More... | |
NMI_API sint8 | m2m_ssl_init (tpfAppSSLCb pfAppSSLCb) |
Initializes the SSL layer. More... | |
NMI_API sint8 | m2m_ssl_retrieve_cert (uint16 *pu16Curve, uint8 *pu8Value, uint8 *pu8Sig, tstrECPoint *pstrKey) |
Retrieve the next set of information from the WINC for ECDSA verification. More... | |
NMI_API sint8 | m2m_ssl_retrieve_hash (uint8 *pu8Value, uint16 u16ValueSz) |
Retrieve the value from the WINC for ECDSA signing. More... | |
NMI_API sint8 | m2m_ssl_retrieve_next_for_verifying (tenuEcNamedCurve *penuCurve, uint8 *pu8Value, uint16 *pu16ValueSz, uint8 *pu8Sig, uint16 *pu16SigSz, tstrECPoint *pstrKey) |
Retrieve the next set of information from the WINC for ECDSA verification. More... | |
NMI_API sint8 | m2m_ssl_send_certs_to_winc (uint8 *pu8Buffer, uint32 u32BufferSz) |
Sends certificates to the WINC. More... | |
NMI_API sint8 | m2m_ssl_set_active_ciphersuites (uint32 u32SslCsBMP) |
Sets the active ciphersuites. More... | |
NMI_API void | m2m_ssl_stop_processing_certs (void) |
Allow SSL driver to tidy up in case application does not read all available certificates. More... | |
NMI_API void | m2m_ssl_stop_retrieving (void) |
Allow SSL driver to tidy up when the application chooses not to retrieve all available information. More... | |