isi_frame_buffer_descriptors Struct Reference
SAMV71/V70/E70/S70 Image Sensor Interface Driver
Frame buffer descriptors.
#include <isi.h>
Data Fields
uint32_t
control
Address of the Control.
More...
uint32_t
current
Address of the Current FrameBuffer.
More...
uint32_t
next
Address of the Next FrameBuffer.
More...
Generated on Fri Mar 4 2022 23:41:22 for OV7740 CMOS image sensor Unit Test for SAMV71-XPRO by
1.8.5