Below is a table listing the acronyms used in this module, along with their intended meanings.
Acronym | Definition |
---|---|
AD | Analog to Digital |
DAC | Digital to Analog Converter |
GPIO | General Purpose Input Output |
NVIC | Nested Vectored Interrupt Controller |
PMC | Power Management Controller |
PWM | Pulse Width Modulator |
QSG | Quick Start Guide |
This driver has the following dependencies:
There are no errata related to this driver.
An overview of the module history is presented in the table below, with details on the enhancements and fixes made to the module since its first release. The current version of this corresponds to the newest version in the table.
Changelog |
---|
Initial document release |