|
void | usart_disable_interrupt (Usart *p_usart, uint32_t ul_sources) |
| Disable USART interrupts. More...
|
|
void | usart_disable_rx (Usart *p_usart) |
| Disable USART receiver. More...
|
|
void | usart_disable_tx (Usart *p_usart) |
| Disable USART transmitter. More...
|
|
void | usart_disable_writeprotect (Usart *p_usart) |
| Disable write protect of USART registers. More...
|
|
void | usart_drive_DTR_pin_high (Usart *p_usart) |
|
void | usart_drive_DTR_pin_low (Usart *p_usart) |
|
void | usart_drive_RTS_pin_high (Usart *p_usart) |
| Drive the pin RTS to 1. More...
|
|
void | usart_drive_RTS_pin_low (Usart *p_usart) |
| Drive the pin RTS to 0. More...
|
|
void | usart_enable_interrupt (Usart *p_usart, uint32_t ul_sources) |
| Enable USART interrupts. More...
|
|
void | usart_enable_rx (Usart *p_usart) |
| Enable USART receiver. More...
|
|
void | usart_enable_tx (Usart *p_usart) |
| Enable USART transmitter. More...
|
|
void | usart_enable_writeprotect (Usart *p_usart) |
| Enable write protect of USART registers. More...
|
|
uint8_t | usart_get_error_number (Usart *p_usart) |
|
uint32_t | usart_get_interrupt_mask (Usart *p_usart) |
| Read USART interrupt mask. More...
|
|
Pdc * | usart_get_pdc_base (Usart *p_usart) |
|
uint32_t * | usart_get_rx_access (Usart *p_usart) |
|
uint32_t | usart_get_status (Usart *p_usart) |
| Get current status. More...
|
|
uint32_t * | usart_get_tx_access (Usart *p_usart) |
|
uint32_t | usart_get_version (Usart *p_usart) |
|
uint32_t | usart_get_writeprotect_status (Usart *p_usart) |
| Get write protect status. More...
|
|
uint32_t | usart_getchar (Usart *p_usart, uint32_t *c) |
| Read from USART Receive Holding Register. More...
|
|
uint32_t | usart_init_hw_handshaking (Usart *p_usart, const sam_usart_opt_t *p_usart_opt, uint32_t ul_mck) |
| Configure USART to work in hardware handshaking mode. More...
|
|
uint32_t | usart_init_irda (Usart *p_usart, const sam_usart_opt_t *p_usart_opt, uint32_t ul_mck) |
|
uint32_t | usart_init_iso7816 (Usart *p_usart, const usart_iso7816_opt_t *p_usart_opt, uint32_t ul_mck) |
|
uint32_t | usart_init_lin_master (Usart *p_usart, uint32_t ul_baudrate, uint32_t ul_mck) |
|
uint32_t | usart_init_lin_slave (Usart *p_usart, uint32_t ul_baudrate, uint32_t ul_mck) |
|
uint32_t | usart_init_lon (Usart *p_usart, uint32_t ul_baudrate, uint32_t ul_mck) |
|
uint32_t | usart_init_modem (Usart *p_usart, const sam_usart_opt_t *p_usart_opt, uint32_t ul_mck) |
|
uint32_t | usart_init_rs232 (Usart *p_usart, const sam_usart_opt_t *p_usart_opt, uint32_t ul_mck) |
| Configure USART to work in RS232 mode. More...
|
|
uint32_t | usart_init_rs485 (Usart *p_usart, const sam_usart_opt_t *p_usart_opt, uint32_t ul_mck) |
| Configure USART to work in RS485 mode. More...
|
|
uint32_t | usart_init_spi_master (Usart *p_usart, const usart_spi_opt_t *p_usart_opt, uint32_t ul_mck) |
| Configure USART to work in SPI mode and act as a master. More...
|
|
uint32_t | usart_init_spi_slave (Usart *p_usart, const usart_spi_opt_t *p_usart_opt) |
| Configure USART to work in SPI mode and act as a slave. More...
|
|
uint32_t | usart_init_sync_master (Usart *p_usart, const sam_usart_opt_t *p_usart_opt, uint32_t ul_mck) |
| Configure USART to work in SYNC mode and act as a master. More...
|
|
uint32_t | usart_init_sync_slave (Usart *p_usart, const sam_usart_opt_t *p_usart_opt) |
| Configure USART to work in SYNC mode and act as a slave. More...
|
|
uint32_t | usart_is_rx_buf_end (Usart *p_usart) |
|
uint32_t | usart_is_rx_buf_full (Usart *p_usart) |
|
uint32_t | usart_is_rx_ready (Usart *p_usart) |
| Check if the received data are ready. More...
|
|
uint32_t | usart_is_tx_buf_empty (Usart *p_usart) |
|
uint32_t | usart_is_tx_buf_end (Usart *p_usart) |
|
uint32_t | usart_is_tx_empty (Usart *p_usart) |
| Check if Transmit Holding Register is empty. More...
|
|
uint32_t | usart_is_tx_ready (Usart *p_usart) |
| Check if Transmit is Ready. More...
|
|
void | usart_lin_abort_tx (Usart *p_usart) |
|
void | usart_lin_disable_checksum (Usart *p_usart) |
|
void | usart_lin_disable_frame_slot (Usart *p_usart) |
|
void | usart_lin_disable_parity (Usart *p_usart) |
|
void | usart_lin_disable_pdc_mode (Usart *p_usart) |
|
void | usart_lin_enable_checksum (Usart *p_usart) |
|
void | usart_lin_enable_frame_slot (Usart *p_usart) |
|
void | usart_lin_enable_parity (Usart *p_usart) |
|
void | usart_lin_enable_pdc_mode (Usart *p_usart) |
|
uint8_t | usart_lin_get_data_length (Usart *usart) |
|
uint8_t | usart_lin_identifier_reception_complete (Usart *usart) |
|
uint8_t | usart_lin_identifier_send_complete (Usart *usart) |
|
uint8_t | usart_lin_read_identifier (Usart *p_usart) |
|
void | usart_lin_send_wakeup_signal (Usart *p_usart) |
|
void | usart_lin_set_checksum_type (Usart *p_usart, uint8_t uc_type) |
|
void | usart_lin_set_data_len_mode (Usart *p_usart, uint8_t uc_mode) |
|
void | usart_lin_set_node_action (Usart *p_usart, uint8_t uc_action) |
|
void | usart_lin_set_response_data_len (Usart *p_usart, uint8_t uc_len) |
|
void | usart_lin_set_tx_identifier (Usart *p_usart, uint8_t uc_id) |
|
void | usart_lin_set_wakeup_signal_type (Usart *p_usart, uint8_t uc_type) |
|
uint8_t | usart_lin_tx_complete (Usart *usart) |
|
void | usart_lon_disable_coll_detection (Usart *p_usart) |
|
void | usart_lon_enable_coll_detection (Usart *p_usart) |
|
uint32_t | usart_lon_is_rx_end (Usart *p_usart) |
|
uint32_t | usart_lon_is_tx_end (Usart *p_usart) |
|
void | usart_lon_set_beta1_rx_len (Usart *p_usart, uint32_t ul_len) |
|
void | usart_lon_set_beta1_tx_len (Usart *p_usart, uint32_t ul_len) |
|
void | usart_lon_set_cdtail (Usart *p_usart, uint8_t uc_type) |
|
void | usart_lon_set_comm_type (Usart *p_usart, uint8_t uc_type) |
|
void | usart_lon_set_data_len (Usart *p_usart, uint8_t uc_len) |
|
void | usart_lon_set_dmam (Usart *p_usart, uint8_t uc_type) |
|
void | usart_lon_set_l2hdr (Usart *p_usart, uint8_t uc_bli, uint8_t uc_altp, uint8_t uc_pb) |
|
void | usart_lon_set_pre_len (Usart *p_usart, uint32_t ul_len) |
|
void | usart_lon_set_priority (Usart *p_usart, uint8_t uc_psnb, uint8_t uc_nps) |
|
void | usart_lon_set_rx_idt (Usart *p_usart, uint32_t ul_time) |
|
void | usart_lon_set_tcol (Usart *p_usart, uint8_t uc_type) |
|
void | usart_lon_set_tx_idt (Usart *p_usart, uint32_t ul_time) |
|
void | usart_man_disable_drift_compensation (Usart *p_usart) |
|
void | usart_man_enable_drift_compensation (Usart *p_usart) |
|
void | usart_man_set_rx_polarity (Usart *p_usart, uint8_t uc_polarity) |
|
void | usart_man_set_rx_pre_len (Usart *p_usart, uint8_t uc_len) |
|
void | usart_man_set_rx_pre_pattern (Usart *p_usart, uint8_t uc_pattern) |
|
void | usart_man_set_tx_polarity (Usart *p_usart, uint8_t uc_polarity) |
|
void | usart_man_set_tx_pre_len (Usart *p_usart, uint8_t uc_len) |
|
void | usart_man_set_tx_pre_pattern (Usart *p_usart, uint8_t uc_pattern) |
|
uint32_t | usart_putchar (Usart *p_usart, uint32_t c) |
| Write to USART Transmit Holding Register. More...
|
|
uint32_t | usart_read (Usart *p_usart, uint32_t *c) |
| Read from USART Receive Holding Register. More...
|
|
void | usart_reset (Usart *p_usart) |
| Reset the USART and disable TX and RX. More...
|
|
void | usart_reset_iterations (Usart *p_usart) |
|
void | usart_reset_nack (Usart *p_usart) |
|
void | usart_reset_rx (Usart *p_usart) |
| Immediately stop and disable USART receiver. More...
|
|
void | usart_reset_status (Usart *p_usart) |
| Reset status bits (PARE, OVER, MANERR, UNRE and PXBRK in US_CSR). More...
|
|
void | usart_reset_tx (Usart *p_usart) |
| Immediately stop and disable USART transmitter. More...
|
|
void | usart_restart_rx_timeout (Usart *p_usart) |
| Restart the receive timeout. More...
|
|
uint32_t | usart_send_address (Usart *p_usart, uint32_t ul_addr) |
| In Multidrop mode only, the next character written to the US_THR is sent with the address bit set. More...
|
|
uint32_t | usart_set_async_baudrate (Usart *p_usart, uint32_t baudrate, uint32_t ul_mck) |
| Calculate a clock divider(CD) and a fractional part (FP) for the USART asynchronous modes to generate a baudrate as close as possible to the baudrate set point. More...
|
|
void | usart_set_rx_timeout (Usart *p_usart, uint32_t timeout) |
| Configure the receive timeout register. More...
|
|
void | usart_set_sleepwalking (Usart *p_uart, uint8_t ul_low_value, bool cmpmode, bool cmppar, uint8_t ul_high_value) |
|
void | usart_set_tx_timeguard (Usart *p_usart, uint32_t timeguard) |
| Configure the transmit timeguard register. More...
|
|
void | usart_spi_force_chip_select (Usart *p_usart) |
| Drive the slave select line NSS (RTS pin) to 0 in SPI master mode. More...
|
|
void | usart_spi_release_chip_select (Usart *p_usart) |
| Drive the slave select line NSS (RTS pin) to 1 in SPI master mode. More...
|
|
void | usart_start_rx_timeout (Usart *p_usart) |
| Start waiting for a character before clocking the timeout count. More...
|
|
void | usart_start_tx_break (Usart *p_usart) |
| Start transmission of a break. More...
|
|
void | usart_stop_tx_break (Usart *p_usart) |
| Stop transmission of a break. More...
|
|
uint32_t | usart_write (Usart *p_usart, uint32_t c) |
| Write to USART Transmit Holding Register. More...
|
|
void | usart_write_line (Usart *p_usart, const char *string) |
| Write one-line string through USART. More...
|
|