Microchip® Advanced Software Framework

Extra Information for Extensible Direct Memory Access Controller Driver

Acronyms

Below is a table listing the acronyms used in this module, along with their intended meanings.

Acronym Definition
AHB AMBA High-performance Bus
AMBA Advanced Microcontroller Bus Architecture
FIFO First In First Out
LLD Linked List Descriptor
QSG Quick Start Guide

Dependencies

This driver has the following dependencies:

  • None

Errata

There are no errata related to this driver.

Module History

An overview of the module history is presented in the table below, with details on the enhancements and fixes made to the module since its first release. The current version of this corresponds to the newest version in the table.

Changelog
Initial document release