|
void | i2s_clear_status (struct i2s_dev_inst *const dev_inst, i2s_interrupt_source_t source) |
| Clear the I2S status value. More...
|
|
void | i2s_disable (struct i2s_dev_inst *const dev_inst) |
| Disable the I2S module. More...
|
|
static void | i2s_disable_clocks (struct i2s_dev_inst *dev_inst) |
| Disable the clocks for the I2S module. More...
|
|
void | i2s_disable_interrupt (struct i2s_dev_inst *const dev_inst, i2s_interrupt_source_t source) |
| Disable the specified interrput sources. More...
|
|
static void | i2s_disable_reception (struct i2s_dev_inst *dev_inst) |
| Disable the I2S module in reception. More...
|
|
static void | i2s_disable_transmission (struct i2s_dev_inst *dev_inst) |
| Disable the I2S module in transmission. More...
|
|
void | i2s_enable (struct i2s_dev_inst *const dev_inst) |
| Enable the I2S module. More...
|
|
static void | i2s_enable_clocks (struct i2s_dev_inst *dev_inst) |
| Enable the clocks for the I2S module. More...
|
|
void | i2s_enable_interrupt (struct i2s_dev_inst *const dev_inst, i2s_interrupt_source_t source) |
| Enable the specified interrput sources. More...
|
|
static void | i2s_enable_reception (struct i2s_dev_inst *dev_inst) |
| Enable the I2S module in reception. More...
|
|
static void | i2s_enable_transmission (struct i2s_dev_inst *dev_inst) |
| Enable the I2S module in transmission. More...
|
|
static void | i2s_get_config_defaults (struct i2s_config *const cfg) |
| Get the default I2S module configuration: Data format: 32 bits Sample frequecny ratio: 1024 Tx channel: Stereo Rx channel: Stereo DMA for Tx: 1 DMA channel for 1 I2S Tx channel DMA for Rx: 1 DMA channel for 1 I2S Rx channel Loopback: No Master mode: Yes Master clock enable: Yes Transmit data in underrun: Yes Slot length is 24: No. More...
|
|
static uint32_t | i2s_get_interrupt_mask (struct i2s_dev_inst *const dev_inst) |
| Get the I2S interrupts mask value. More...
|
|
static uint32_t | i2s_get_status (struct i2s_dev_inst *dev_inst) |
| Get the I2S status value. More...
|
|
enum status_code | i2s_init (struct i2s_dev_inst *const dev_inst, I2sc *i2sc, struct i2s_config *const cfg) |
| Initialize and configure the I2S module. More...
|
|
enum status_code | i2s_read (struct i2s_dev_inst *dev_inst, uint32_t *data) |
| Read a single message of data. More...
|
|
static void | i2s_reset (struct i2s_dev_inst *dev_inst) |
| Resets the I2S module. More...
|
|
void | i2s_set_callback (struct i2s_dev_inst *const dev_inst, i2s_interrupt_source_t source, i2s_callback_t callback, uint8_t irq_level) |
| Set callback for I2S. More...
|
|
enum status_code | i2s_write (struct i2s_dev_inst *dev_inst, uint32_t data) |
| Write a single message of data. More...
|
|