Microchip® Advanced Software Framework

Extra Information for DAC Driver

Acronyms

The table below presents the acronyms used in this module:

Acronym Description
ADC Analog-to-Digital Converter
AC Analog Comparator
DAC Digital-to-Analog Converter
LSB Least Significant Bit
MSB Most Significant Bit
DMA Direct Memory Access

Dependencies

This driver has the following dependency:

Errata

There are no errata related to this driver.

Module History

An overview of the module history is presented in the table below, with details on the enhancements and fixes made to the module since its first release. The current version of this corresponds to the newest version in the table.

Changelog
Initial Release