Microchip® Advanced Software Framework

Extra Information for PAC Driver

Acronyms

Below is a table listing the acronyms used in this module, along with their intended meanings.

Acronym Description
AC Analog Comparator
ADC Analog-to-Digital Converter
EVSYS Event System
NMI Non-Maskable Interrupt
NVMCTRL Non-Volatile Memory Controller
PAC Peripheral Access Controller
PM Power Manager
RTC Real-Time Counter
SERCOM Serial Communication Interface
SYSCTRL System Controller
TC Timer/Counter
WDT Watch Dog Timer

Dependencies

This driver has the following dependencies:

  • None

Errata

There are no errata related to this driver.

Module History

An overview of the module history is presented in the table below, with details on the enhancements and fixes made to the module since its first release. The current version of this corresponds to the newest version in the table.

Changelog
Initial Release