Microchip® Advanced Software Framework

Extra Information for RTC (CAL) Driver

Acronyms

Below is a table listing the acronyms used in this module, along with their intended meanings.

Acronym Description
RTC Real Time Counter
PPM Part Per Million
RC Resistor/Capacitor

Dependencies

This driver has the following dependencies:

  • None

Errata

There are no errata related to this driver.

Module History

An overview of the module history is presented in the table below, with details on the enhancements and fixes made to the module since its first release. The current version of this corresponds to the newest version in the table.

Changelog
Added support for RTC tamper feature
Added driver instance parameter to all API function calls, except get_config_defaults
Updated initialization function to also enable the digital interface clock to the module if it is disabled
Initial release