Microchip® Advanced Software Framework

Extra Information for SYSTEM INTERRUPT Driver

Acronyms

The table below presents the acronyms used in this module:

Acronym Description
ISR Interrupt Service Routine
NMI Non-maskable Interrupt
SERCOM Serial Communication Interface

Dependencies

This driver has the following dependencies:

  • None

Errata

There are no errata related to this driver.

Module History

An overview of the module history is presented in the table below, with details on the enhancements and fixes made to the module since its first release. The current version of this corresponds to the newest version in the table.

Changelog
Initial Release