Below is a table listing the acronyms used in this module, along with their intended meanings.
Acronym | Description |
---|---|
ADC | Analog-to-Digital Converter |
DAC | Digital-to-Analog Converter |
LSB | Least Significant Bit |
MSB | Most Significant Bit |
DMA | Direct Memory Access |
This driver has the following dependencies:
There are no errata related to this driver.
An overview of the module history is presented in the table below, with details on the enhancements and fixes made to the module since its first release. The current version of this corresponds to the newest version in the table.
Changelog |
---|
Added support for SAM R21 |
Added support for SAM D21 and new DMA quick start guide |
Added ADC calibration constant loading from the device signature row when the module is initialized |
Initial Release |