The supported board list:
- SAMD21 Xplained Pro
- SAMR21 Xplained Pro
- SAML21 Xplained Pro
- SAML22 Xplained Pro
- SAMDA1 Xplained Pro
- SAMC21 Xplained Pro
- SAMHA1G16A Xplained Pro
In this use case, the I2C will used and set up as follows:
- Slave mode
- 100KHz operation speed
- Not operational in standby
- 65535 unknown bus state timeout value
Prerequisites
The device must be connected to an I2C slave.
Setup
Code
The following must be added to the user application:
- Address to respond to:
- A sample buffer to send, number of entries to send and address of slave:
- Globally accessible module structure:
- Function for setting up the module:
- Globally accessible DMA module structure:
- Globally accessible DMA transfer descriptor:
- Function for setting up the DMA resource:
- Function for setting up the DMA transfer descriptor:
- Add to user application
main()
:
Workflow
- Configure and enable module:
- Create and initialize configuration structure.
- Change settings in the configuration.
- Initialize the module with the set configurations.
- Enable the module.
- Configure DMA
- Create a DMA resource configuration structure, which can be filled out to adjust the configuration of a single DMA transfer.
- Initialize the DMA resource configuration struct with the module's default values.
- Note
- This should always be performed before using the configuration struct to ensure that all values are initialized to known default settings.
- Set extra configurations for the DMA resource. It is using peripheral trigger. SERCOM RX trigger causes a beat transfer in this example.
- Allocate a DMA resource with the configurations.
- Create a DMA transfer descriptor configuration structure, which can be filled out to adjust the configuration of a single DMA transfer.
- Initialize the DMA transfer descriptor configuration struct with the module's default values.
- Note
- This should always be performed before using the configuration struct to ensure that all values are initialized to known default settings.
- Set the specific parameters for a DMA transfer with transfer size, source address, and destination address.
- Create the DMA transfer descriptor.
Implementation
Code
Add to user application main()
:
Workflow
- Start to wait a packet from master.
- Once data ready, clear the address match status.