Common Standard I/O Serial Management.
This file defines a useful set of functions for the Stdio Serial interface on SAM0 devices.
Copyright (c) 2009-2018 Microchip Technology Inc. and its subsidiaries.
Variables | |
void(* | ptr_get )(void volatile *, char *) |
Pointer to the external low level read function. More... | |
int(* | ptr_put )(void volatile *, char) |
Pointer to the external low level write function. More... | |
volatile void *volatile | stdio_base |
Pointer to the base of the USART module instance to use for stdio. More... | |