Microchip® Advanced Software Framework

Extra Information for DMAC Driver

Acronyms

Below is a table listing the acronyms used in this module, along with their intended meanings.

Acronym Description
DMA Direct Memory Access
DMAC Direct Memory Access Controller
CPU Central Processing Unit

Dependencies

This driver has the following dependencies:

Errata

There are no errata related to this driver.

Module History

An overview of the module history is presented in the table below, with details on the enhancements and fixes made to the module since its first release. The current version of this corresponds to the newest version in the table.

Changelog
Add SAM C21 support
Add SAM L21 support
Add SAM R30 support
Initial Release