Microchip® Advanced Software Framework

Extra Information for NVM Driver

Acronyms

The table below presents the acronyms used in this module:

Acronym Description
NVM Non-Volatile Memory
EEPROM Electrically Erasable Programmable Read-Only Memory

Dependencies

This driver has the following dependencies:

  • None

Errata

There are no errata related to this driver.

Module History

An overview of the module history is presented in the table below, with details on the enhancements and fixes made to the module since its first release. The current version of this corresponds to the newest version in the table.

Changelog
Removed BOD12 reference, removed nvm_set_fuses() API
Added functions to read/write fuse settings
Added support for NVM cache configuration
Updated initialization function to also enable the digital interface clock to the module if it is disabled
Initial Release