semphr.
h
void vSemaphoreDelete( xSemaphoreHandle xSemaphore );
Delete a semaphore. This function must be used with care. For example, do not delete a mutex type semaphore if the mutex is held by a task.
xSemaphore | A handle to the semaphore to be deleted. |
h
void vSemaphoreDelete( SemaphoreHandle_t xSemaphore );
Delete a semaphore. This function must be used with care. For example, do not delete a mutex type semaphore if the mutex is held by a task.
xSemaphore | A handle to the semaphore to be deleted. |