Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
vTaskResumeFromISR

task.

h

void xTaskResumeFromISR( xTaskHandle xTaskToResume );

INCLUDE_xTaskResumeFromISR must be defined as 1 for this function to be available. See the configuration section for more information.

An implementation of vTaskResume() that can be called from within an ISR.

A task that has been suspended by one of more calls to vTaskSuspend () will be made available for running again by a single call to xTaskResumeFromISR ().

Parameters
xTaskToResumeHandle to the task being readied.

h

void xTaskResumeFromISR( TaskHandle_t xTaskToResume );

INCLUDE_xTaskResumeFromISR must be defined as 1 for this function to be available. See the configuration section for more information.

An implementation of vTaskResume() that can be called from within an ISR.

A task that has been suspended by one or more calls to vTaskSuspend () will be made available for running again by a single call to xTaskResumeFromISR ().

xTaskResumeFromISR() should not be used to synchronise a task with an interrupt if there is a chance that the interrupt could arrive prior to the task being suspended - as this can lead to interrupts being missed. Use of a semaphore as a synchronisation mechanism would avoid this eventuality.

Parameters
xTaskToResumeHandle to the task being readied.
Returns
pdTRUE if resuming the task should result in a context switch, otherwise pdFALSE. This is used by the ISR to determine if a context switch may be required following the ISR.

h

void xTaskResumeFromISR( xTaskHandle pxTaskToResume );

INCLUDE_xTaskResumeFromISR must be defined as 1 for this function to be available. See the configuration section for more information.

An implementation of vTaskResume() that can be called from within an ISR.

A task that has been suspended by one of more calls to vTaskSuspend () will be made available for running again by a single call to xTaskResumeFromISR ().

Parameters
pxTaskToResumeHandle to the task being readied.